This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Sign in to access this content and additional site features.
Pedro Lopez from RTI talks about how they are enabling the software-defined vehicle (SDV) with ECU consolidation using a data-centric framework with dynamic data sharing (DDS) middleware running on the NXP S32G processor. RTI provides a level of abstraction using the DDS standard to make it easier to move processing from the edge of the vehicle to a gateway. A demonstration shows how a vehicle zone with a microcontroller connected to GNSS and camera sensors can be processed in the S32G gateway/vehicle computer. The RTI software is available as part of the NXP S32G Vehicle Integration Platform (GoldVIP). Close collaboration between NXP hardware and RTI software helps customers transition to SDVs.
Start designing with the NXP S32G vehicle network processors.