201811011I:PCA85233 Datasheet Device Initialization & Setup
  • Product Change Notification (PCN)
  • 201811011I

201811011I : PCA85233 Datasheet Device Initialization & Setup

Added sections 7.4.1 "Device Initialization" and 7.4.2 "Device Setup" to the PCA85233 DS as follows: 7.41 Device InitializationAt power-on the status of the I2C-bus communication interface is undefined since this device doesn't have POR which was removed to improve the ESD performance. A START and STOP condition with dummy byte in-between must be sent after every power reset to set up the I2C-bus communication interface.Also added the following note to the 3rd bullet of section 7.4.1 "Device Initialization" outline:"Note this is not the device address but just a dummy byte of all zeros."7.42 Device SetupAt power-on the status of the display and configuration registers are undefined and need to be set up to properly display information on the LCD display. After the I2C-bus interface is initialized as discussed in 7.41 set up the device using these register settingsAlso added the following note to the last bullet of section 7.4.2 "Device Setup" outline:"or left off (blank) with bit E = 0." Note: CIN #201811011I will be added to the "Revision History" section of the new PCA85233_5_20181108 DS uploaded in the "Files" section once the CIN is approved & distributed.

PCN Type Change Category Issue Date Effective Date
Customer Information Notification Errata 16-Nov-2018 17-Nov-2018

Reason of Change

The intend of these changes is to make the PCA85233 DS easier to follow when initializing and setting up the device.

Identification of Affected Products

Product identification does not change

Anticipated Impact

Data sheet revision: A new datasheet will be issued

These datasheet changes does not affect the PCA85233 product functionality. No impact on form fit function reliability or quality.

Affected Parts

Part Number / 12NC Last Time Buy Date Last Time Delivery Date Replacement Part
PCA85233UG/2DA/Q1Z
(935302508033)
- - -