1
Get Started2
Get to Know the Hardware3
Configure the HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the PTN38007/ PTN38003 evaluation board.
The kit contents include:
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Something went wrong! Please try again.
Something went wrong! Please try again.
There are two boards included in the EVM package: a H2 board and a D2 board. The H2 board (or DFP board) is intended to plug into a notebook or PC and connect to a device via a USB-C cable. The D2 board (or UFP board) is intended to plug into a device or monitor and connect to a notebook or PC via a USB-C cable.
An included USB-2-I²C module is used to configure the EVM via a GUI running on a host PC.
PTN38007 EVMs can be used to evaluate USB3, DisplayPort, Thunderbolt3 and USB4 interfaces. The PTN38003A EVMs can only support USB3 and DisplayPort interfaces.
Something went wrong! Please try again.
PTN38007/3 P2R application board and LPCUSBSIO module should be connected together such that J103
is mated with J307
, and J104
is
mated with J306
. Use J101
to connect to host side, and J102
to connect to device side.
A micro-USB cable should be connected to J301
on the LPCUSBSIO module to provide power to the entire setup. This USB cable allows the use of NXPs LPCUSBSIO
USB-2- I²C bridge to communicate with PTN38007/3’s I²C via USB2 interface. The user can download PTN38007/PTN38003A GUI from the Design Resources
section of this guide. It is recommended to first flash the LPCUSBSIO module with the latest firmware, which is located under the GUI package firmware directory. Refer
to UM11595 for details on how to flash the firmware.
In the GUI package, there are directories for H2 board (PTN3800x DFP) and D2 board (PTN3800x UFP). Execute the GUI that matches the correct hardware. There are default script files that are already pre-loaded in each directory based on the hardware type. If the wrong script directory is used, the EVM is configured incorrectly.
Connect with other engineers and get expert advice on designing with the PTN38003 evaluation board on one of our community sites.