Getting Started with the KITPF5200SKTEVM Evaluation Board | NXP Semiconductors

Getting Started with the KITPF5200SKTEVM Evaluation Board

Last Modified: Apr 18, 2023Supports PF5200 Socketed Evaluation Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Get Software
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the KITPF5200SKTEVM board.

1.1 Kit Contents and Packing List

The KITPF5200SKTEVM contents include:

  • Assembled and tested evaluation board and preprogrammed FRDM-KL25Z microcontroller board in an anti-static bag
  • 3.0 ft USB-STD A to USB-B-mini cable
  • Jumpers mounted on board
  • Quick Start Guide
  • 1.2 Additional Hardware

    In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

    • Power supply with a range of 3.3 V to 5.0 V and a current limit set initially to 1.0 A

    1.3 Windows PC Workstation

    This reference design requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.

    • USB-enabled computer with Windows 7 or Windows 10

    1.4 Software

    Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITPF5200SKTEVM.

    • PF5200 NXP GUI installation package

    2. Get Hardware

    2.1 Board Features

    • Banana 4 mm for power supply input
    • Banana 4 mm for switcher 1 and switcher 2
    • TBBEN and PWRON
    • PGOOD, RESETBMCU and XFAIL pins
    • USB to I²C protocol for easy connection to software GUI
    • LEDs, green and red, that indicate signal or regulator status
    • LED blue to indicate that VDDOTP pin is set to 8.0 V (OTP burning voltage)
    • HWQFN32 socket to plug and play with PF5200

    2.2 Board Description

    The KITPF5200SKTEVM kit provides an integrated platform for evaluating designs based on NXP’s PF5200 dual-channel PMIC. All PF5200 features can be accessed and monitored in a test environment. Limitation related to the PF5200 socket restrict current to 1.0 A.

    The kit hardware consists of the KITPF5200SKTEVM evaluation board, a FRDM-KL25Z microcontroller board and the USB cable required to connect the FRDM-KL25Z to the PC.

    2.3 Kit Featured Components

    Figure 1 shows the location of key KITPF5200SKTEVM components.

    Position Function Description
    J1/J4 VIN Input voltage (3.3 V min / 5.5 V max)
    J1/J4 SW1OUT Output for SW1
    J3/J6 SW2OUT Output for SW2
    SW1 VIN switch PWRON manual control (assume J12 on PWRON_SW position)
    J9 TBBEN_SEL Apply either V1P5D or 3.3 V from MCU or GND to TBBEN pin
    J10 VIN_IC Apply VIN to VIN IC pin
    J12 PWRON_SEL PWRON controlled either by the MCU or manually by SW1
    J14 VDDIO_EN Apply VDDIO to VDDIO pin
    J16 VDDIO_SEL VDDIO set to either 1.8 V or 3.3 V
    J22 PGOOD_SEL PGOOD setting either PGGO/GPO or output of temperature junction analog voltage

    2.4 Kinetis KL25Z Freedom Board

    The Freedom KL25Z is an ultra low-cost development platform for Kinetis L series MCU built on Arm Cortex-M0+ processor.

    3. Get Software

    The KITPF5200SKTEVM is delivered with the GUI firmware already flashed. If your MCU firmware is already flashed, you can ignore this section. If you need to update the firmware or it is malfunctioning, follow the instructions detailed in the following sections.

    3.1 Flashing the FRDM-KL25Z Firmware – Windows 7

    If BOOTLOADER is already loaded on the FRDM-KL25Z board, skip Step 1 and Step 2 and start with Step 3.

    1. Press the RST push-button and plug the USB cable into the SDA port on the FRDM-KL25Z board
      • A new “BOOTLOADER” device appears on the left pane of the File explorer
    2. Locate the file MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA from the package and drag and drop into the BOOLTLOADER device
    3. Disconnect and reconnect the USB cable into the SDA port
      • This time without pressing the RST push-button, the FRDM_KL25Z device should appear on the left pane of the File explorer as shown in the following figure
    4. Locate the file “nxp-gui-fw-frdmkl25z-usb_hid-pf5200_v0.9.bin” from the package and drag and drop the file into the FRDM_KL25Z device
    5. Freedom board firmware is successfully loaded. Disconnect the USB cable from the SDA port and reconnect it to the FRDM-KL25Z USB port

    3.2 Flashing the FRDM-KL25Z Firmware – Windows 10

    1. Disable the storage services: run the services, double-click on the storage service from the list and press the Stop button

      If BOOTLOADER is already loaded on the FRDM-KL25Z board, skip Step 2 and Step 3 and start with Step 4.

    2. Press the RST push-button and plug the USB cable into the SDA port on the Freedom board
      1. A new “BOOTLOADER” device should appear on the left pane of the File explorer
    3. Drag and drop the file “MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA” into the BOOTLOADER drive
    4. Disconnect and reconnect the USB cable into the SDA port
      • This time without pressing the RST push-button, the FRDM_KL25Z device should appear on the left pane of the File explorer as shown in the following figure
    5. Locate the file nxp-gui-fw-frdmkl25z-usb_hid-pf5200_v0.8.bin from the package and drag and drop the file into the FRDM_KL25Z device
    6. Freedom board firmware is successfully loaded. Disconnect the USB cable from the SDA port and reconnect it into the KL25Z USB port

    4. Configure Hardware

    4.1 Configure Hardware

    The procedure for setting up the KITPF5200SKTEVM board is as follows:

    1. Make sure that the board has the jumpers configured in their default positions as shown in Figure 3. The default configuration enables the board to be fully controlled by the FRDM-KL25Z and the GUI
    2. Connect the power supply to J1 (VIN) and J4 (GND). The power supply should be set to an initial value of 5.0 V and current limited to 1.0 A
    3. Verify that the FRDM-KL25Z board is firmly mounted to the KITPF5200SKTEVM board. Also, make sure that the USB cable between the FRDM-KL25Z and the PC is securely connected. This connection is critical because the USB port not only serves as a communication channel between the PC and the FRDM-KL25Z board, but also provides voltages and references to some onboard circuits and generates the VDDIO reference for the IC