Getting Started with the KITFS86SKTFRDMEM Evaluation Board | NXP Semiconductors

Getting Started with the KITFS86SKTFRDMEM Evaluation Board

Last Modified: 2021-11-18 13:35:00Supports KITFS86SKTFRDMEM: FS86 Safety SBC Programming Socket Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Get Software
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the KITFS86SKTFRDMEM board.

1.1 Kit Contents and Packing List

The KITFS86SKTFRDMEM contents include:

  • Assembled and tested KITFS86SKTFRDMEM connected to a FRDM-KL25Z in an antistatic bag
  • 3.0 ft USB-STD A to USB-B-mini cable
  • Two connectors, terminal block plug, 2 pos., str. 3.81 mm
  • Two connectors, terminal block plug, 3 pos., str. 3.81 mm
  • Jumpers mounted on board
  • Quick Start Guide

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

  • Power supply with a range of 8.0 V to 60 V and a current limit set initially to 1.0 A

1.3 Windows PC Workstation

This reference design requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.

  • USB-enabled computer with Windows 7 or Windows 10

1.4 Software

Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITFS86SKTFRDMEM or from the provided link.

2. Get Hardware

2.1 Board Features

  • VBAT power supply connectors (Jack and Phoenix)
  • VPRE output capability up to 1.0 A (socket limit)
  • VBUCK 1.0 V to 3.3 V
  • VBOOST 5.0 V to 6.0 V
  • LDO1 1.5 V to 5.0 V
  • LDO2 1.1 V to 5.0 V
  • Ignition key switch
  • FS0B external safety pin
  • Embedded USB connection for easy connection to software NXP GUI (access to I²Cbus, IOs, RSTB, FS0B, INTB, Debug, MUX_OUT, regulators, register access, OTP emulation and programming)
  • LEDs that indicate signals and regulator status
  • Support OTP fuse capabilities
  • Voltage monitoring jumper setting

2.2 Board Description

The KITFS86SKTFRDMEM enables development on FS8600 family of devices. The kit can be connected to the NXP GUI software which allows you to play with registers, try OTP configurations and burn the part.

The devices can be placed and removed easily from the board by using the socket. The device OTP can be burned twice, which provides a good flexibility. This board supports FS86 family of devices.

2.3 Board Components

Number Description
1 LDO1 / LDO2 power supply
2 BUCK / BOOST power supply
3 VBAT Jack connector
4

VBAT three position switch

  • Left position: board supplied by Jack connector
  • Middle position: board not supplied
  • Right position: board supplied by Phoenix connector
5 VBAT Phoenix connector
6 VPRE power supply
7 USB connectors (Open SDA for MCU flash; KL25Z for NXP GUI control)
8 Debug connectivity. Access to FS8600 signals
9 External regulator connectors (to VMONx)
10 VMONx configuration (Choice between monitoring a regulator or a fixed 0.8 V)
11 OTP mode switch
12 DBG pin to 0 V if unplugged
13 Wake1 switch
14 VPRE compensation network settings (455 kHz or 2.22 MHz)
15 VDDI2C selection
16 KL25Z Freedom board connectors

2.4 Kinetis KL25Z Freedom Board

The Freedom KL25Z is an ultra low-cost development platform for Kinetis L series MCU built on Arm Cortex-M0+ processor.

3. Get Software

3.1 Install the Software

The device configuration can be programmed twice and emulated indefinitely using the GUI.

Device programming and emulation steps are described in the NXP GUI for FS86 Automotive Family User Manual available at NXP GUI for Automotive PMIC Families.

4. Configure Hardware

4.1 Configure the Hardware

4.2 Hardware Configuration

Switch Configuration
Normal mode Debug mode entry OTP mode entry
Operation watchdog 2s window watchdog window fully open OTP emulation / programming and Debug mode entry
J7 (DBG) open connect 1 to 2 DBG pin voltage pulled to 4.5 V or 8.0 V (SW3)
SW1 (WAKE1) close (WAKE1 high)
SW2 (VBAT) middle position (VBAT OFF)
SW3 (DBG_OTP) open (DBG = 4.5 V) close (OTP mode ON)

To configure the hardware and workstation as illustrated in Figure 3, complete the following procedure:

  1. Install jumpers and switches for the configuration shown in Table 2
  2. Connect the Windows PC USB port to the KITFS86SKTFRDMEM development board using the provided USB 2.0 cable
  3. Set the DC power supply to 12 V and current limit to 1.0 A. With power turned off, attach the DC power supply positive and negative output to VBAT Phoenix connector (J6)
  4. Turn on the power supply
  5. Put SW2 in TOP position

At this step, if the product is in OTP mode entry configuration, all regulators are off. The user can power up with an OTP configuration or configure the mirror registers before powering up. Power-up starts as soon as one of these four actions occurs:

  • J7 jumper is removed
  • SW3 is switched off
  • OTP mode exit command is sent by I²C
  • NXP GUI button "Exit OTP Mode" is clicked