Getting Started with the KITFS85FRDMEVM | NXP Semiconductors

Getting Started with the KITFS85FRDMEVM

Last Modified: 2020-08-24 12:40:38Supports KITFS85FRDMEVM

Contents of this document

  • 1

    Get Started
  • 2

    Get the Hardware
  • 3

    Configure Hardware
  • 4

    Install Software

1. Get Started

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the KITFS85FRDMEVM evaluation board.

1.1 Kit Contents and Packing List

The KITFS85FRDMEVM contents include:

  • Assembled and tested evaluation board in an antistatic bag
  • 3.0 ft USB-STD A to USB-B-mini cable
  • Two connectors, terminal block plug, 2 pos., str. 3.81 mm
  • Three connectors, terminal block plug, 3 pos., str. 3.81 mm
  • Jumpers mounted on board
  • Quick Start Guide

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

  • Power supply with a range of 8.0 V to 40 V and a current limit set initially to 1.0 A (maximum current consumption can be up to 6.0 A)

1.3 Windows PC Workstation

This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.

  • USB-enabled computer with Windows 7 or Windows 10

1.4 Software

Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITFS85FRDMEVM.

  • FlexGUI latest version
  • FS85_FS84_OTP_Config.xlsm
  • Java Installation

2. Get to Know the Hardware

2.1 Board Features

  • VBAT power supply connectors (Jack and Phoenix)
  • VPRE output capability up to 6.0 A (external MOSFET)
  • VBUCK1/2 in standalone (default) or multiphase mode, up to 3.6 A peak
  • VBUCK3 up to 3.6 A peak
  • VBOOST 5.0 V or 5.74 V, up to 400 mA
  • LDO1 and LDO2, from 1.1 V to 5.0 V, up to 400 mA
  • Ignition key switch
  • FS0B external safety pin
  • Embedded USB connection for easy connection to software GUI (access to SPI/I2C bus, IOs, RSTB, FS0B, INTB, Debug, MUX_OUT, regulators)
  • LEDs that indicate signal or regulator status
  • Support OTP fuse capabilities
  • USB connection for register access, OTP emulation and programming

2.2 Board Description

The KITFS85FRDMEVM provides flexibility to play with all the features of the device and make measurements on the main part of the application. The KL25Z MCU installed on the board, combined with the FlexGUI software allows access to the registers in read and write mode. All regulators are accessible through connectors. Nonuser signal, like DC/DC switcher node is mapped on test points. Digital signals (SPI, I2C, RSTB, etc.) are accessible through connectors. WAKE1 pin has a switch to control (Ignition) them. A VBAT switch is available to power ON or OFF the device.

This board can be operated in Emulation mode or in OTP mode. In emulation mode, as long as the power is supplied, the board configuration stays valid. The OTP mode uses the fused configuration. The device can be fused three times. In OTP mode, the device always starts with the fused configuration, except if the user wants to overwrite OTP configuration using Emulation mode. This board is able to fuse the OTP without any extra tools or boards.

2.3 Board Components

Number Description
1 VBAT Jack connector.
2 VBAT three position switch:
  • Left position: board supplied by Jack connector
  • Middle position: board not supplied
  • Right position: board supplied by Phoenix connector
3 VBAT Phoenix connector.
4 LDO1/LDO2 power supply.
5 VPRE power supply.
6 BUCK1/BUCK2 power supply.
7 USB connector (for FlexGUI control).
8 Debug connectivity. Access to:
  • VSUP, GND
  • FOUT/FIN
  • PGOOD/RSTB/FS0B
  • FCCUx
  • WAKE2
  • PSYNC, ERRMON, AMUX
  • VMONx
9 Programming. Access to:
  • SPI bus
  • I2C-bus
  • Debug pin
  • VPRE, VSUP, GND
10 WAKE1 switch.
11 OTP burning voltage switch.
12 VBOOST and BUCK3 power supply.
13 Debug voltage source either from USB (recommended) or from VSUP.
14 FIN frequency selection.

3. Configure Hardware

3.1 Configure the Hardware

To configure the hardware and workstation, complete the following procedure:

  1. Install jumpers for the configuration
    Jumper Configuration
    J9 Connect 1-2 (Connect 5.0 V on DBG pin from the USB).
  2. Configure switches for the configuration
    Switch Configuration
    SW3 Middle position (VBAT OFF)
    SW1 Open (OTP programming OFF)
    SW2 Open (WAKE1)
  3. Connect the Windows PC USB port to the KITFS85FRDMEVM development board using the provided USB 2.0 cable
  4. Set the DC power supply to 12 V and current limit to 1.0 A. With power turned OFF, attach the DC power supply positive and negative output to KITFS85FRDMEVM VBAT Phoenix connector (J1)
  5. Turn ON the power supply
  6. Close SW2

4. Install Software

This development kit uses FlexGUI software. FlexGUI software is based on Java JRE. Preparing the Windows PC workstation consists of three steps:

  1. Install the appropriate Java SE Runtime Environment (JRE)
  2. Install the Windows 7 FlexGUI driver
  3. Install the FlexGUI software package

4.1 Install the Java JRE

  1. Download Java JRE (Java SE Runtime Environment), available at Java Downloads  (8u162 or newer)
  2. Open the installer and follow the installation instructions
  3. Following the successful installation, restart the computer

4.2 Install Windows 7 FlexGUI driver

On Windows 7 PCs, a virtual COM port installation is required. Install the Windows 7 FlexGUI driver using the following procedure.

  1. Connect the kit to the computer as described in Section 3 "Configure Hardware"
  2. On the Windows PC, open the "Device Manager"
  3. In the "Device Manager" window, right-click on "SECON FLEX GUI SLAVE" and then select "Properties"
  4. In the "SECON FLEX GUI SLAVE Properties" window, click "Update Driver"
  5. In the "Update Driver Software" window, select "Browse my computer for driver software"
  6. Select "Let me pick from a list of device drivers on my computer" and then click Next
  7. Select "Ports (COM and LPT)" from the list and then click Next
  8. Click "Have Disk"
  9. Click "Browse"
  10. In the "Locate File" window, locate and select fsl_ucwxp and then click Open
  11. In the "Install from Disk" window, click OK
  12. If prompted in the "Windows Security" window, click "Select this driver software anyway"
  13. Close the window when the installation is complete
  14. In the "Virtual Com Port Properties" window, verify that the device is working properly and then click Close
  15. The Virtual COM Port appears in the "Device Manager" window

4.3 Install FlexGUI software package

The FlexGUI software installation requires only extracting the zip file in a desired location.

  1. If necessary, install the Java JRE and Windows 7 FlexGUI driver
  2. Download the latest FlexGUI (32-bit or 64-bit) version, available at KITFS85FRDMEVM
  3. Extract all the files to a desired location on your PC

FlexGUI is started by running the batch file: \bin\flexgui-app-fs85.bat.

4.4 Success

Now, start your embedded application development.