1
Get Started2
Get Hardware3
Install Software4
Configure HardwareSign in to save your progress. Don't have an account? Create one.
NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KITFS5600SKTEVM evaluation board.
The KITFS5600SKTEVM contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITFS5600SKT-EVM.
Refer to the user manual under Design Resources for additional details on featured component and board configurations.
Something went wrong! Please try again.
Something went wrong! Please try again.
The KITFS5600SKTEVM is a hardware evaluation tool that allows performance test and OTP programming of the FS5600.
An Emulation mode is possible to test different OTP configurations as needed. Different inductors and MOSFETs are included in the kit to allow the user to try different switching frequencies.
Something went wrong! Please try again.
Unzip the NXPGUI_PR_x into any desired location. Find the NXP_GUI_x.x-Setup from the GUI folder inside the package and run it to install the GUI in any desired location.
Something went wrong! Please try again.
For Windows 10, disable the storage services: run services.msc; double-click on the storage service from the list and press the Stop button.
J5
) on the Freedom board Note: Make sure to allow enough time for the firmware to be saved in the Bootloader. The device should change to FRDM_K82FD.
To use the hardware configuration:
To use the software GUI configuration:
J5
(via an included 10-pin ribbon cable)Something went wrong! Please try again.
Figure 1. Presents a typical hardware configuration incorporating the development board, power supply and Windows PC workstation.
To configure the hardware and workstation as illustrated in Figure 1, complete the following procedure:
J21
and J25
Something went wrong! Please try again.