Getting Started with the i.MX93 EVK | NXP Semiconductors

Getting Started with the i.MX93 EVK

Last Modified: 2023-04-04 12:46:00Supports i.MX 93 Evaluation Kit

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Build, Run

1. Out of the Box

Video Player is loading.
Current Time 0:00
Duration 1:43
Loaded: 9.60%
Stream Type LIVE
Remaining Time 1:43
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected
  • en (Main), selected

The following section describes the steps to boot the i.MX 93 EVK.

Development kit contains:

  • i.MX 93 EVK board along with M.2 module with NXP’s Wi-Fi 6 Tri-radio IW612
  • Power Supply: USB Type-C 45W power delivery supply, 5 V/3 A; 9 V/3 A; 15 V/3 A; 20 V/2.25 A supported
  • Cable: Assembly, USB 2.0, Type-C male to Type-A male
  • Software: Linux BSP image programmed in eMMC
  • Quick start guide

Get started on developing your application on the i.MX 93 EVK by referring to the out-of-the-box video, available at i.MX 93 applications processor documentation.

1.1 Get Familiar With the Board

Top view i.MX 93 11x11 EVKCM board

Top view i.MX 93 11x11 EVKCM board

1.2 Boot From eMMC

The i.MX 93 EVK comes with a pre-built NXP Linux binary demo image flashed on the eMMC. Without modifying the binary inside, booting from the eMMC provides a default system with certain features for building other applications on top of Linux.

To understand more about NXP's Embedded Linux®, MCUXpresso SDK, continue reading the next sections.

1.3 Connect USB Debug Cable

Connect the supplied USB Type-C cable to the debug UART port J1401, then connect the other end of the cable to a host computer.

Four UART connections will appear on the host computer. The third port is for A55 core and the fourth port is for M33 core system debugging.

If you are unfamiliar with terminal applications, please view one of the following tutorials before continuing to step 1.4: Minicom Tutorial, Tera Term Tutorial, PuTTY Tutorial.

1.4 Connect the HDMI Cable

To see the user interface provided with the image binary, connect a monitor via the MIPI-DSI J701 with IMX-MIPI-HDMI cable.

1.5 Boot Switch Setup

Please refer to i.MX 93 EVK Quick Start Guide.

1.6 Connect Power Supply

Connect the power supply cable to the power connector (J301).

Power the board by flipping the switch (SW1301).

The processor starts executing from the on-chip ROM code. With the default boot switch setup, the code reads the fuses to define the media where it is expected to have a bootable image. After it finds a bootable image, the U-Boot execution should begin automatically.

Information is printed in the serial console for the Arm® Cortex®-A55. If you do not stop the U-Boot process, it continues to boot the kernel.

Congratulations, Linux Boot is complete.

As the board boots up, you will see 2 penguins appear in the upper left-hand corner of the monitor, and then you will see the Linux terminal Icon on the top left and timer on right top corner. Congratulations, you are up and running.

2. Get Software

This section is applicable ONLY if attempting to load a Linux® operating system on the board.

The i.MX Linux board support package (BSP) is a collection of binary files, source code and support files that are used to boot an Embedded Linux image on a specific i.MX development platform.

Current releases of Linux binary demo files can be found on the i.MX Linux download page. Additional documentation is available in the i.MX Linux documentation bundle under the Linux sections of the i.MX Software and Development Tools.

2.1 Overview

Before the Linux OS kernel can boot on an i.MX board, the Linux kernel is loaded to a boot device (SD card, eMMC and so on) and the boot switches are set to boot that device.

There are various ways to download the Linux BSP image for different boards and boot devices.

This Getting Started guide only outlines a few methods of transferring the Linux BSP to an SD card. Experienced Linux developers can explore other options if desired.

2.2 Download an NXP Linux BSP Pre-Built Image

The latest pre-built images for the i.MX 93 EVK are available on the Linux download page under the most current version on Linux.

The pre-built NXP Linux binary demo image provides a typical system and basic set of features for using and evaluating the processor. Without modifying the system, the users can evaluate hardware interfaces, test SoC features and run user space applications.

When more flexibility is desired, an SD card can be loaded with individual components (boot loader, kernel, dtb file and rootfs file) one-by-one or the *wic image is loaded and the individual parts are overwritten with the specific components.

2.3 Burn NXP Linux BSP Image Using Universal Update Utility (UUU)

In addition to the connections from "Out of the Box" section, connect the USB1 to the host machine using the proper USB cable.

Turn off the board. Refer to the "1.5 Boot Switch Setup" section and configure the board to boot on serial download protocol (SDP) mode.

Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary. Choose an option below for detailed instructions:

3. Build, Run

The MCUXpresso software development kit (MCUXpresso SDK) provides comprehensive software source code to be executed in the i.MX 93 M33 core. If you do not wish to enable the Arm® Cortex®-M33 on i.MX 93 at this moment you can skip this section.

3.1 Overview

The MCUXpresso SDK is designed for the development of embedded applications for Cortex®-M33 standalone or collaborative use with the A cores. Along with the peripheral drivers, the MCUXpresso SDK provides an extensive and rich set of example applications covering everything from basic peripheral use case examples to demo applications. The MCUXpresso SDK also contains RTOS kernels and device stack and various other middleware to support rapid development.

This guide shows how to run the m33_image.bin demo provided by the REL_2.13.0 release. For detailed information on MCUXpresso SDK and how to build and deploy custom demos, please visit MCUXpresso SDK site.

3.2 Run Applications Using U-Boot

This section describes how to run applications using an SD card and pre-built U-Boot image for i.MX processor.

  1. Following the steps from section 2. Get Software, prepare an SD card with a pre-built U-Boot + Linux image from the Linux BSP package for the i.MX 93 processor. If you have already loaded the SD card with a Linux image, you can skip this step.
  2. Insert the SD card in the host computer (Linux or Windows) and copy the application image (for example m33_image.bin) to the FAT partition of the SD card.
  3. Safely remove the SD card from the PC.
  4. Insert the SD card to the target board. Make sure to use the default boot SD slot and double check the boot switch setup guide.
  5. Connect the DEBUG UART connector on the board to the PC through a USB cable. The Windows OS installs the USB driver automatically, and the Ubuntu OS will find the serial devices as well.

    See Connect USB debug cable section for more instructions on serial communication applications. Open a second terminal on the i.MX93 EVK board's second enumerated serial port.

  6. This is the Cortex-M33's serial console. Set the speed to 115200 bit/s, data bits 8, 1 stop bit (115200, 8N1), no parity.
  7. Power up the board and stop the boot process by pressing any key before the U-Boot countdown reaches zero. At the U-Boot prompt on the first terminal, type the following commands.
    1234=> fatload mmc 1:1 0x80000000 m33_image.bin
    => cp.b 0x80000000 0x201e0000 0x10000
    => bootaux 0x201e0000
    

    These commands copy the image file from the partition of the SD card into the Cortex-M33's TCM and releases the Cortex-M33 from reset.

Minicom Tutorial

Serial Communication Console Setup

On the command prompt of the Linux host machine, run the following command to determine the port number:

1$ ls /dev/ttyUSB*

The smaller number is for Arm® Cortex®-A55 core and the bigger number is for Arm Cortex-M33 core.

Minicom

Use the following commands to install and run the serial communication program (minicom as an example):

  • Install Minicom using Ubuntu package manager
  • 1$ sudo apt-get install minicom
  • Launch Minicom using a console window using the port number determined earlier
  • 1$ sudo minicom /dev/ttyUSB* -s
  • Configure Minicom as show in Figure
  • The next step is to Connect the HDMI cable.

Tera Term Tutorial

Serial Communication Console Setup

The FTDI USB-serial chip on i.MX 93 enumerates 4 serial ports. Assume that the ports are COM11,COM12,COM13,COM14. The third Port(COM13) is for the serial console communication from Arm® Cortex®-A55 core and the fourth port(COM14) is for Arm Cortex-M33 core. The serial-to-USB drivers are available at FTD Chip Drivers.

Tera Term

Is an open source terminal emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.

  • Download Tera Term. After the download, run the installer and then return to this webpage to continue
  • Launch TeraTerm. The first time it launches, it shows the following dialog. Select the serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list
  • Configure the serial port settings (using the COM port number identified earlier) to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup → Serial Port and change the settings
  • Verify that the connection is open. If connected, Tera Term shows something like below in its title bar
  • The next step is to Connect the HDMI cable

Putty Tutorial

Serial Communication Console Setup

TThe FTDI USB-serial chip on i.MX 93 enumerates 4 serial ports. Assume that the ports are COM11,COM12,COM13,COM14. The third Port(COM13) is for the serial console communication from Arm® Cortex®-A55 core and the fourth port(COM14) is for Arm Cortex-M33 core. The serial-to-USB drivers are available at FTD Chip Drivers

PuTTY is a popular terminal-emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.

  • Download PuTTY After the download, run the installer and then return to this webpage to continue.
  • Launch PuTTY by either double clicking on the executable file you downloaded or from the Start menu, depending on the type of download you selected.
  • Configure In the window that launches. Select the Serial radio button and enter the COM port number that you determined earlier. Also enter the baud rate, in this case 115200.
  • Click Open to open the serial connection. Assuming the board is connected and you entered the correct COM port, the terminal window opens. If the configuration is not correct, PuTTY alerts you.
  • The next step is to Connect the HDMI cable.