Getting Started with the FRDM-K82F | NXP Semiconductors

Getting Started with the FRDM-K82F

Last Modified: 2020-08-31 19:00:29Supports FRDM-K82F | K82/K81/K80 | Wireless

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run
  • 4

    Create

1. Plug It In

Let's take your FRDM-K82F for a test drive! You have the choice of watching the sequence in a short video or following the detailed actions list below.

1.1 Getting Started with FRDM-K82F Development Platform

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected

      1.2 Attach the USB Cable

      FRDM-K82F-GS-BOARD

      FRDM-K82F-GS-BOARD

      1.3 Run the Out-of-Box Demo

      Your FRDM-K82F comes loaded with a "bubble level" demo that leverages the on-board accelerometer. When the board is flat, the RGB LED is turned off, and when the board is tilted, the green or blue LEDs gradually illuminate based on the degree of tilt on the X- and Y-Axis.

      FRDM-K82F-DEMO

      FRDM-K82F-DEMO

      2. Get Software

      2.1 Installing Software for the FRDM-K82F

      Video Player is loading.
      Current Time 0:00
      Duration 0:00
      Loaded: 0%
      Stream Type LIVE
      Remaining Time 0:00
       
      1x
      • Chapters
      • descriptions off, selected
      • captions off, selected

          2.2 Jump Start Your Design with the Kinetis SDK

          The Kinetis Software Development Kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software. Learn about SDK.

          Click below to download the K82F SDK package.

          Get Kinetis SDK

          2.3 Install Your Toolchain

          NXP offers a complimentary toolchain called Kinetis Design Studio (KDS).

          Get Kinetis Design Studio

          Want to use a different toolchain?

          No problem! The Kinetis SDK includes support for other tools such as IAR , Keil  and command-line GCC .

          2.4 PC Configuration

          Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged in to your PC.

          Download Driver

          With the serial port driver installed, run your favorite terminal application to view the serial output from the MCU's UART. Configure the terminal to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the FRDM-K82F's virtual COM port, open the device manager and look under the "Ports" group.

          Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.

          3. Build, Run

          3.1 Build and Run SDK Demos on the FRDM-K82F

          Video Player is loading.
          Current Time 0:00
          Duration 0:00
          Loaded: 0%
          Stream Type LIVE
          Remaining Time 0:00
           
          1x
          • Chapters
          • descriptions off, selected
          • captions off, selected

              3.2 Explore the SDK Example Code

              The Kinetis SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select your board, the FRDM-K82F: <sdk_install_directory>/boards/frdmk82f.

              To learn more about specific example code, open the readme.txt file in an example's directory.

              3.3 Build, Run and Debug SDK Examples

              If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with Kinetis SDK guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.

              Use the guide below to learn how to open, build and debug an example application using the Kinetis Design Studio (KDS) IDE.

              Using a different toolchain?

              4. Create

              4.1 Create an Application for the FRDM-K82F

              Video Player is loading.
              Current Time 0:00
              Duration 0:00
              Loaded: 0%
              Stream Type LIVE
              Remaining Time 0:00
               
              1x
              • Chapters
              • descriptions off, selected
              • captions off, selected

                  4.2 Get SDK Project Generator

                  Let's create our own project and make a simple SDK-based application. NXP provides an intuitive, simple project generation utility that allows creation of custom projects based on the Kinetis SDK.

                  Get SDK Project Generator

                  4.3 Run the SDK Project Generator

                  After extracting the ZIP file, open the utility by clicking on the KSDK_Project_Generator executable for your computer's operating system. Point the tool to your SDK installation path, name your project, and select the board that it uses as a reference. Click on the Quick Generate button to finish.

                  FRDM-K82F-KSDK-PROJECT-GENERATOR

                  FRDM-K82F-KSDK-PROJECT-GENERATOR.

                  4.4 Open Your Project

                  Your new project will be located in <sdk_install_directory>/examples/frdmk82/user_apps. Open the project in your toolchain of choice by using the same process described in Section 3.2.

                  4.5 Write Some Code

                  Now, let's make our new project do something other than spin in an infinite loop. The SDK examples provide a board support package (BSP) to do various things specific to the board, including macros and definitions for items such as LEDs, switches and peripheral instances. To keep things simple, lets make the LED blink using the BSP macros.

                  Update the main() function in your project's main.c file with the following code:

                  12345678910111213141516171819202122volatile uint32_t delay;
                      
                  BOARD_InitPins();
                  BOARD_BootClockRUN();
                  BOARD_InitDebugConsole();
                  
                  PRINTF("myProject project\n\r);
                  
                  // Enable the clock to the PORT module that the LED is on
                  CLOCK_EnableClock(kCLOCK_PortD);
                  
                  // Set the PORT configuration - from DISABLED → GPIO
                  PORT_SetPinMux(BOARD_LED_GREEN_GPIO_PORT, BOARD_LED_GREEN_GPIO_PIN, kPORT_MuxAsGpio);
                  
                  // Initialize the green LED
                  LED_GREEN_INIT(LOGIC_LED_OFF);
                  for (;;)
                    {
                        LED_GREEN_TOGGLE();
                        delay = 5000000;
                        while (delay--);
                    }

                  4.6 Build, Download, Run

                  With the changes made to your main() function, build your application. Remember to build the SDK platform library first if you did not build any of the other SDK examples in the previous steps. Once the build is complete, download the application to your board.

                  If you need help figuring out how to build, download or run an application, reference your tool-specific guide from Section 3.2.

                  4.7 Success

                  With the application downloaded, you will see the FRDM-K82's red LED blinking. You can also view terminal output using PRINTF.