Compact List
The NXP® Advanced Diode model is an extension to normal diode models to include a much better description of especially the reverse behavior. The model includes the following physical mechanisms:
As a result of these extra descriptions also the temperature behavior has also drastically improved, without the need for an extra temperature scaling parameter.
The source code of Advanced Diode model is available here. The file "pmk_device_d500.c" contains the majority of the Advanced Diode model. Please notice that the file is located in the directory source/pmk. If you use the included solver, please make sure that you compile on a system that supports Fortran 77.
The models are included in a dynamically loaded library called SiMKit. SiMKit is related to the following circuit simulators used within NXP:
The Advanced Diode level 500 is not available for the ADS simulator.
Quick reference to our documentation types
1 document
Compact List
There are no results for this selection.
Please wait while your secure files are loading.
1 documents
Compact List
There are no recently viewed products to display.
Help us improve your experience on our site. We invite you to take our five-question survey.