What do you get when five companies come together to address key challenges facing the development
and production deployment of connected intelligent vehicles? You get The Fusion Project—a
pre-integrated hardware, software and cloud solution combining their innovative technologies to
efficiently collect, analyze and manage connected vehicle data with support for machine learning
model training and deployment for continuous vehicle improvements. While providing an end-to-end
solution supporting the data management lifecycle, the realization cost and model training time is
dramatically reduced while maintaining high model accuracy with low latency.
To know more about
Connected data lifecycle
click here
The Vehicle Data Opportunity
As
vehicles
have advanced with new technologies and sensors, the amount of available data is exponentially
increasing. This data can be used to power new data-centric features and continual vehicle
improvements for consumers and revenue-generating opportunities for automakers. However,
efficiently collecting, analyzing and managing vehicle data presents unique challenges to
automakers.
The Challenges
Simply put, it’s because of fragmented data management across the machine learning lifecycle,
static machine learning models, limited capabilities in intelligent edge computing and
insufficient in-vehicle computing power. On top of this, other approaches are not optimized to
extend to production vehicles which is key to realizing the promise of vehicles that improve over
time.
An All-In-One Solution
So, in comes The Fusion Project, which pre-integrates technologies from five companies into a
solution that automakers can easily evaluate and introduce into vehicle design and production
cycles for next generation connected and autonomous vehicles. The five companies –
Airbiquity®, Cloudera, NXP® Semiconductors, Teraki™ and Wind
River® - combine the complex technologies and expertise required to provide an
end-to-end solution that otherwise would require several man-years. It offers substantial new
capabilities and efficiency improvements while reducing automotive OEM and Tier 1 development
efforts.
First Use Case
The first application for The Fusion Project implements intelligent vehicle lane change detection
using synergistic technologies from each company. This is a key use case required to support
increased vehicle automation from lane keep to lane change maneuvers and on to fully autonomous
driving applications. The company contributions include:
- Airbiquity – Over-the-Air (OTA) Software Management
- Cloudera – Data Lifecycle Solutions from Edge to AI
- NXP – Vehicle Processing Platforms
- Teraki – Edge Data Artificial Intelligence (AI)
- Wind River – Intelligent Edge System Software
The complete data management lifecycle between the intelligent vehicle edge to the cloud
highlighting each company’s contributions is shown in the figure below.

Airbiquity, Cloudera, NXP, Teraki and Wind River have opened the door for future intelligent
connected vehicle use cases to cost-effectively access key vehicle data, train machine learning
models in the cloud and deploy them to vehicles for continuous improvements.
The sky’s the limit for The Fusion Project, or in this case, the road is endless.
Learn more about The Fusion Project visiting
CLOUDERA also, you can take our
Enabling Connected Intelligent Vehicles with The Fusion Project Machine Learning-Based Data
Lifecycle on-demand training.
Discover how this multiparty automotive industry technology collaboration defines a data
lifecycle platform for enabling and optimizing future connected and autonomous vehicle
systems.