Water | NXP Semiconductors

Recycled Water

We implement projects that collect and recycle water at our manufacturing sites. This reduces the amount of incoming water consumption, reduces our reliance on local water supplies and makes our operations more efficient. Since 2015, our percentage of water recycling has increased by 14 percentage points, and 4 percentage points compared to 2023. As of year-end 2024, we recycled 55% of our water and have created a task force to identify opportunities for water recycling, so we can achieve our 2027 goal of 60% recycled water.

Wastewater

We are committed to returning water to the environment that is as clean as, or cleaner than, what we sourced. We employ onsite water-treatment facilities to treat wastewater outflows and ensure any chemical constituents from our wastewater that could potentially impact the environment are avoided. Our Facility Teams continuously monitor and test our water, as required by local authorities, and aim to discharge wastewater that is cleaner than what local regulations require.

Note: NXP did not receive any excursions, fines or penalties in 2024 related to wastewater discharge.

Wastewater Discharge Unit 2022 2023 2024
Total Wastewater Discharge m3 8,775,035 8,896,447 9,437,200