Important: This page contains secure information about our products. Sign in to access authorized resources.
Important: This page contains secure information about our products.
View Secure InformationImportant: To include authorized secured information please reenter your password.
SIGN INAt NXP, our goal is to provide you with environmentally preferred products that meet both regulatory requirements and your specific restrictions on hazardous substances and minerals. Below you will find answers to some of the most common questions about NXP’s products and links to details.
NXP has programs in place that support both initiatives. More can be found in our NXP Semiconductors RoHS Declaration .
The symbol indicates the product is EU/CN RoHS Compliant. We certify that, to the best of our knowledge, these products meet the requirements of the European Union's Restriction on Use of Hazardous Substances in Electrical and Electronic Equipment (RoHS) Directive 2011/65/EU, and can therefore be called EU RoHS compliant. These products have lead-free terminations and do not make use of an exemption under the EU RoHS directive. These products also meet the requirements of the Chinese ACPEIP (Administration on the Control of Pollution Caused by Electronic Information Products), the "China RoHS". NXP cannot warrant that our customer’s products, which incorporate NXP products, will in turn comply with the European Union's Directive 2011/65/EU and/or with the Chinese ACPEIP.
The symbol indicates the product is EU RoHS Compliant. We certify that, to the best of our knowledge, these products meet the requirements of the European Union's Restriction on Use of Hazardous Substances in Electrical and Electronic Equipment (RoHS) Directive 2011/65/EU and can therefore be called EU RoHS compliant. These products have lead-free terminations but use an exemption under the EU RoHS directive. This includes, for example, products with lead in high-melting-temperature solders used for die-attach or glass-diodes containing lead. NXP cannot warrant that our customer’s products, which incorporate NXP products, will in turn comply with the European Union's Directive 2011/65/EU.
We comply with the guidelines of the initiative and give details in our explanatory statement on REACH provisions .
NXP products (semiconductor devices, evaluation modules and used packaging materials) manufactured or sold by NXP Semiconductors do not contain any of the substances currently on Annex XIV ("Authorization List") published by ECHA. Furthermore, NXP products do not contain any of the substances above the maximum limits under the given applications of Annex XVII of the REACH Regulation (EC) 1907/2006. Under these conditions our products are "REACH compliant". When ECHA adds new substances to the candidate lists of SVHC, NXP will work to identify possible inclusions of SVHC in NXP products. Based upon the results of these investigations the explanatory statement on REACH provisions will be updated by NXP. For further explanation please review the NXP explanatory statement on REACH provisions .
We recognize the health hazard of lead and work to eliminate it from our operations. We pursue environmental improvement, including the reduction or elimination of the potential hazardous effects from lead poisoning, and promote lead-free manufacturing, a practice that is mandated by legislation and supported by strong market demand.
A product can be deemed Pb-Free if it contains less than 1000 ppm Pb by weight of homogeneous material. See more detailed info under the topic RHF-indicator, below.
This logo appears on the barcode label if the product does not contain any lead and thus conforms with the Pb-Free definition. The barcode label is attached to both the reel and the box. Where possible, the reel label is the same size as the PQ label. When the label is too large for the reel, the PQ label is cut in two, with the bottom half placed on the front of the reel and the top half on the rear.
Yes. For many years our products have been suitable for the higher temperature profiles required by most lead-free soldering processes. Because all lead-free devices have either pure tin or NiPdAu plating, we ensure full forward and backward compatibility. The only exception is the BGA family, since conventional reflow temperatures are too low for melting SAC solder balls. As with any change, it may be necessary to re-optimize the soldering processes when switching to a lead-free option.
All dimensions, as well mechanical and electrical behavior are unaffected. Also, no change in the distribution of electrical parameters has been detected.
NXP is a charter member of the Die Attach 5 (or DA5) consortium. Through the DA5, NXP has been working with key suppliers since 2009 to define industry requirements for Pb-Free alternatives, to evaluate supplier materials and to develop feasible manufacturing processes for consistently reliable products. For more information, click here to review the DA5 Project Presentation .
For our small-signal discrete products, there is no impact on the MSL. For ICs, about 70% of cases experience no change, while the remaining 30% are likely to have some change in MSL. Please review the individual package listing for more detailed information.
No. Guaranteed shelf life remains the same as for current SnPb products.
After many years of experience, NXP has found pure tin to be the proven, logical choice for coating package leads and terminals, since it enables ideal drop-in replacements for devices using lead-alloy platings.
Along with thorough test procedures, the following measures are introduced into the production process:
NXP, as a main supplier of semiconductor products to the electronics industry, is promoting halogen-free manufacturing. Currently there is already a wide range of NXP halogen-free products available on the market.
A product is deemed halogen-free if it contains less than 900 ppm of chlorine or bromine compounds by weight of homogeneous material, and less than 1500 ppm combined bromine and chlorine compounds. The halogens fluorine, iodine and astatine are not in scope. In addition, content is also less than 900 ppm for antimony oxides by weight of homogeneous material. See more detailed info under the RHF-indicator, below.
This logo is added to the barcode label if the product does not contain any halogens and thus conforms to the Halogen-Free definition. The barcode label is attached to both the reel and the box. Where possible, the Reel label is the same size as the Product Quality label. When the label is too large for the reel, the PQ label is cut in two, with the bottom half placed on the front of the reel and the top half on the rear.
RHF stands for RoHS Halogen Free. NXP introduced the RHF-2006 indicator to identify compliance and it is used in the marking of commercial products and on their packing labels. RHF-2006 identification codes are as follows:
RHF-2006 indicator | Description |
---|---|
Dark Green = Indicates products that fully comply with the EU Directive 2011/65/EU (RoHS) without exemptions and halogens and Antimony Oxides. | |
Green = Indicates products that fully comply with the EU Directive 2011/65/EU (RoHS) without exemptions, but containing halogens and/or Antimony Oxides. | |
Halogen and Antimony Oxide-Free, Leaded = Indicates products that comply with the EU Directive 2011/65/EU (RoHS) with exempted Lead, but Halogen and Antimony Oxide Free as well. | |
Exempt, Leaded = Indicates products that comply with the EU Directive 2011/65/EU (RoHS) with exempted lead, and also containing halogens and/or Antimony Oxides. | |
Non-EU/CN RoHS compliant = Indicates all non-RoHS compliant products, whether or not they contain halogens or Antimony Oxides. This includes products with lead in the outer terminals, such as QFP with traditional SnPb plating, and BGAs with SnPb balls. |
When a product is identified as Green (G), it implies that it is RoHS compliant using the following limits:
Substances | Threshold limit |
Cadmium | • < 100 ppm (0.01%) • |
Lead | < 1000 ppm (0.1 %) |
Mercury, Chromium (VI), PBB's and PBDE's | < 1000 ppm (0.1 %) |
Phthalates (BBP, DBP, DEHP and DIBP) | < 1000 ppm (0.1 %) • |
The substances listed above are not intentionally added, but may be present as an impurity with an upper limit according to the listed values. Threshold limits refer to the individual homogeneous materials (such as post-plating, adhesive, substrate, mould compounds, etc.).
RHF stands for RoHS Halogen Free. NXP introduced the RHF-2006 indicator to identify compliance and it is used in the marking of commercial products and on their packing labels. RHF-2006 identification codes are as follows:
Substances | Threshold limit |
Antimony Oxides (as Sb) | < 900 ppm (0.09%)1 |
Chlorinated compounds (as Cl) | < 900 ppm (0.09%) |
Brominated compounds (as Br) | < 900 ppm (0.09%) |
Σ (Chlorinated + Brominated compounds) | < 1500 ppm (0.15%) |
1In glass diodes | < 1500 ppm (0.15%) |
The substances listed above are not intentionally added, but may be present as an impurity with an upper limit according to the listed values. Exception is made for glass diodes, where a substance has been intentionally added due to its critical application as a fining agent (or degasser) to reduce the number of air bubbles in the glass. Threshold limits refer to the individual homogeneous materials (such as post-plating, adhesive, substrate, die encapsulants etc.).
The RHF-indicator can be found in our package/quality information on our product summary pages. Look for the 'PACKAGE/QUALITY' button in the top right of those pages. These are accessible via the search box in the right top corner of the NXP Home Page. When searching for a specific product you can select the part number from the provided table. To get to the Package/Quality page please use the link provided in the pop-up window our use one of the other links and then click on the "Package/Quality" tab.
EU RoHS includes exemptions for certain uses of lead (Pb) within semiconductor products. NXP packages such as flip chip (with Pb bumps for die attach), high power (with high Pb solder die attach), and sensors (with Pb glass frit die) contain lead above the RoHS maximum allowable concentration limit (1000 ppm by weight of homogeneous material), therefore are not "Pb-Free", but still considered EU RoHS compliant under the applicable RoHS exemption for the usage of lead.
The 2nd level interconnect categories are published on the Product Composition Declarations which can be accessed via the Environmental Product Compliance Documentation Search website.
The J-STD-609 standard defines the following categories:
Yes. Most NXP products will indicate Lead-free status, RoHS compliance status, Halogen-Free status, if applicable, as well as Moisture Sensitivity Level (MSL) and Peak Package Body Temperature (PPT) on shipping labels. The part number is also marked on packing labels.
NXP targets a PPT of 260 °C with an MSL of 3 or better, however, some products may not be able to meet this target. NXP provides the PPT and MSL level for each part number via web access or by special request.
We are here to answer any inquiries regarding environmental product compliance.