Green and next-generation mobility is turning out to be a key factor in the automotive industry
bounce back after Covid-19. With record Electric Vehicle sales forecast for 2021, governments and
investor interest in forward-looking mobility technologies have opened the door to funding and
incentives to continue sweetening the move to electric.
The transport sector, responsible for around 24% of CO2 emissions globally, is fully in the
environmental spotlight, and governments are pushing ahead with ever stricter regulations on
vehicle emissions. Norway is at the more aggressive end of the scale, planning to phase out all
new sales of internal combustion engine, (ICE), passenger cars by 2025. In the rest of Europe,
targets vary between 2030 and 2040, and China is aiming for a minimum 50% market share of New
energy vehicles (NEVs) by 2035.
The global automotive sector is responding to these looming emissions deadlines, with all major
manufacturers, including Volvo, Daimler, Volkswagen and Ford announcing massive investments in EV
development programs. Led by Tesla, the market leader with almost 30% of global sales in the first
half of 2020, global automakers collectively launched 143 new EVs in 2019 and plan to introduce
another 450 models by 2022.

Perhaps one of the biggest barriers to EV adoption thus far has been consumer perception over EV
price and performance limitations, especially range; the distance a vehicle can travel before the
battery needs to be recharged. These perceptions are progressively eroded as charging
infrastructure increases and the industry invests heavily in improving EV development, with a
strong focus on battery technology and efficiency improvement.
The modern automobile contains a number of advanced electronic subsystems, each responsible for
controlling specific functionality, such as ADAS, infotainment, functional safety and drivetrain,
including battery management. The architecture of these onboard systems has evolved away from
multiple electronic control units (ECUs) to a collection of domains, each managed by domain
controllers which share data and collaborate with each other. These domain controllers are based
on powerful, embedded microcontrollers which enable complex processing, using advanced techniques
such as virtualization, formerly the preserve of datacentre-based servers.
The impact of this onboard processing capability increases exponentially thanks to developments in
vehicle connectivity. C-V2X technology leverages the improved performance and coverage of cellular
networks to share the massive amounts of data generated by the car and its sensors, (up to 4
Terabytes per hour), to the cloud. This shared data enables a number of value-adding use cases,
including insurance, fleet management, preventative diagnostics and intrusion detection. The
connected car also brings the power of cloud-edge processing and artificial intelligence to
enhance the power of the onboard domain controllers.

The ongoing quest to improve vehicle efficiency and range is driving significant research and
development in the propulsion control domain, where energy optimization is a key challenge. A
hybrid-electric vehicle (HEV) can optionally be powered by its ICE or its electric motor, and the
vehicle’s range is directly dependent on the optimal use of these energy sources. Powerful control
algorithms within the propulsion controller decide which source to use, where to use the ICE,
where to use the electric motor and where regenerative braking can be used to increase the battery
charge state. The quality of these decisions, which directly affect the vehicles range, is
enhanced when the controller has access to cloud-based contextual information such as precise
location, traffic conditions, average speed of route, expected duration of journey, charging
stations locations, gradients on the planned route and driver style.
Vehicle connectivity also enables energy optimization to be enhanced by cloud-edge processing
techniques, where deep learning frameworks train machine learning (ML) models in the cloud. These
ML models are deployed to the domain controller in the vehicle (the edge) where they use a process
known as inferencing to make predictions based on real-time data generated from the vehicle’s
sensors.
To integrate the power of this technology, vehicle manufacturers require access to specialist
knowledge backed by in-depth resources and NXP Semiconductors are one of a select number of
organizations in the ecosystem with this capability. A global leader in auto microprocessors,
ADAS, radar, secure car access, infotainment and in-vehicle networking, the NXP comprehensive
solution portfolio enables our customers to accelerate the design of their next generation
automotive designs, enabling rapid time to market and scalability.
We have a strong track record working with some of the world’s largest vehicle manufacturers to
deliver high performance, safe and reliable mobile solutions. To learn more about our specific
capabilities, read our whitepaper “
Using Vehicle to Cloud Connectivity to Extend Electric Vehicle Range” on our website.