Author

Vanessa Lowe
Vanessa Lowe has been with NXP for over 5 years, in various marcom and communications roles. She is responsible for Global Sales Communications, as well as on the core team for NXP's social media strategy.
Sign in for a personalized NXP experience.
NFC technology and tags have been around for a few years now, but for the most part people do not realize the full potential of the technology. The most popular use for the tags is to turn on Bluetooth while in the car, but there are so many other great uses for the tags. Here, NXP shares the 20 best and most creative uses for the technology.
1) Save Battery
Wifi, Bluetooth and other external sources can drain your phone’s battery. Place a tag by your bed that is programmed to turn off these battery-draining accessories while you sleep.
2) As an Alarm
Are you constantly in a battle with your phone’s snooze button? Stick a tag to your coffee machine or in your bathroom so that you’re required to get out of bed to turn it off. Bonus- have a tag programmed to pull up your favorite social media to get updated while you drink your coffee.
3) Send a Message
Send your loved one a daily “Good Morning” message by programming your NFC tag to do so. Have the tag near your bed so that it’s the first thing you do when you wake up. Get brownie points without having to think about it!
4) Sleep like a Baby
If you’re a light sleeper, have a tag toggle your phone from vibrate to silent, allowing you a peaceful night’s sleep. In the morning, tap the phone back to the tag to return it to the original settings.
5) Hit the Gym
Stick a tag to your gym bag to automatically turn your phone in airplane mode so that you’re not interrupted in the middle of a run with phone calls or text messages. Program the tag to also begin playing your favorite workout playlist.
6) Sell Something
Trying to sell your bike? Find a job as a babysitter? When making your flyers to post to bulletin boards, include an NFC tag that connects to the Ebay site or your Sitter City profile.
7) Raise Money for a Cause
While you’re out posting flyers, why not raise some money for the cause that you’re passionate about? Having an event for your philanthropy? Include a tag that provides more information about the cause and links to a donation site. Or are you hosting a race or sports event for charity? Along the same lines, have a tag with your flyer that sends people to the registration page.
8) Make Class Easier
NFC tags can’t necessarily do your work for you, but it can certainly streamline the learning environment. How often do you lose your syllabus or misplace your teacher’s email the day you’re sick? With an NFC tag by the door, the syllabus, contact info and even links to purchase the books can be downloaded instantly.
9) Share your Info
Keep a programmed tag in your wallet or purse that allows people to connect to your Facebook, twitter, Instagram and other social media. No longer struggle with searching through 20 different Kevin Smiths to find the one you met. Just a tap, and you’re friends.
10) Quick Dial
Have some contacts that you frequently call while driving? Program some tags that place a call to that specific person. Stick the tag somewhere in your car, and enjoy the ease of being hands free!
11) Don’t Text and Drive
Use a tag to respond to people while driving- program the tag to automatically send a message in response to the last text received that states “I’m driving, text you later,” allowing you to focus on the road.
12) Sync with your Car
As stated in the beginning, syncing Bluetooth with an NFC tag is pretty common knowledge. However, it’s still an awesome ability and worth mentioning. Place a tag in your car that automatically syncs Bluetooth and opens Pandora for a seamless driving experience.
13) Share your Wifi
Instead of sharing your personal password (which is most likely used as a password for other things as well, many people reuse passwords), have an NFC tag that allows your guests to access your Wifi without giving them your password.
14) Lock and Unlock your Door
Lockitron is a smart door lock that can be locked and unlocked with your NFC enabled smartphone. No longer hassle with keys- simply use your phone to access your home. Also, settings allow for certain users to gain access, such as friends or family members.
15) Command like a Jedi
Did you get that NFC enabled lock? Feel like a Jedi Leader by opening the door
just using your fingers- with an NFC enabled ring! The NFC Ring has two
different NFC chips; one on the inside for private data, such as the lock, and
one on the outside for public sharing, such as Facebook connections or contact
information. The NFC Ring also allows for the unlocking of the phone, and
triggering other NFC tags and devices!
16) Have the most Tech-Chic Manicure
For DIY tech-lovers, make your own NFC manicure. Take apart a tag, careful to keep the antenna untangled and place it onto your thumb or pointer finger with a bonding agent and cover the tag with a gel shellac nail polish. Program the tag to open your phone, or to share your contact information with just a touch.
17) Ditch the Wallet
Payment is starting to go mobile, thanks to NFC technology. Already
we’re seeing it being used in contactless cards, but soon even cards
themselves will be extinct. NFC enabled phones are able to securely store
credit card information and pay for goods by simply tapping the phone on the
payment terminal.
18) Learn Something New
NFC enabled smart posters are on trend right now, and certainly will only continue to rise. See a nice pair of sunglasses in an advertisement? Tap your phone to the tag to pull up the website for details and to order them. Or, go above and beyond for a class project by including a tag on your project poster that engages classmates in an interactive learning experience.
19) Share Photos
Samsung just released its new camera- the NFC enabled NX series. Now you can easily transfer photographs from the camera to your phone with just a tap, satisfying the need to instantly upload to social media sites or share with loved ones through email. Have a friend with an NFC enabled phone? Bump your phones to share photographs, playlists or sync for a game.
20) Turn on Electronics
More and more companies are producing NFC enabled devices, such as stereos or gaming devices. Tapping the phone to the device not only turns it on, but syncs your music via Bluetooth and allows for seamless playing. Get that party started!
There is a vast variety of uses for NFC technology. Share your creative uses of NFC tags with us on our Twitter @NXP and #NFCeverywhere
Tags: Security, Technologies
Digital Marketing Communications Manager, NXP Semiconductors
Vanessa Lowe has been with NXP for over 5 years, in various marcom and communications roles. She is responsible for Global Sales Communications, as well as on the core team for NXP's social media strategy.
September 19, 2019
October 23, 2019
by Davina Moore
February 28, 2020
by Kurt Sievers