Sign in for a personalized NXP experience.
The Federal Information Processing Standard (FIPS 140-3) Level 3 certification makes it easier to design secure IoT and industrial devices, providing differentiation with advanced security capabilities and features, and ensures eligibility to participate in federal projects.
NXP Semiconductors today announced the EdgeLock SE052F, the industry’s first hardware secure element certified for the newest FIPS 140-3 Level 3 standard. Part of the proven EdgeLock SE05x family, the EdgeLock SE052F combines the flexibility of a secure element with the newest generation of the Federal Information Processing Standard (FIPS), a U.S. and Canadian federal standard for data security required by NIST for participation in federal projects. In addition, this standard has become an indicator of advanced security capabilities. This makes it easier to design secure and differentiated devices across the IoT and industrial markets, while also improving time to market.
As security becomes increasingly important for smart connected devices, many industrial IoT device manufacturers are turning to certifications, such as Common Criteria or FIPS, as a differentiator for their design, even outside of national or federal contracts, demonstrating advanced security features and capabilities. Using the FIPS 140-3 L3 certified EdgeLock SE052F secure element makes it easier for manufacturers to meet the requirements of the standard, accelerating time to market and reducing costs.
“The EdgeLock SE052F allows us to push the limit of edge device security within the physical security industry. The solution enables new Axis network cameras, access control, intercom and audio products to meet the FIPS 140-3 security requirements for cryptographic modules.”
Johan Paulsson, CTO at network security technology specialists Axis Communications
“Security is crucial to the success of the IoT. The EdgeLock SE052F enables hassle-free and flexible trust provisioning and FIPS certification for our customers, allowing them to bring differentiated products to market more quickly.”
Alasdair Ross, Senior Director, NFC IoT Security, NXP
The EdgeLock SE052F secure element is both FIPS 140-3 L3 and Common Criteria EAL 6+ certified and offers flexible memory management and extended memory (100kb). It also features cryptographic functionalities, such as ECDSA and ECDH/E based on NIST and Brainpool curves, RSA up to 4K (including key generation), and authenticated AES encryption modes CCM/GCM. The EdgeLock SE052F is supported by EdgeLock 2GO, offering remote key management and follows the Plug & Trust approach used by all EdgeLock secure elements and secure authenticators. NXP’s Plug & Trust approach ensures a complete product support package and provides example codes for a broad range of use cases to support a fast and easy design-in process.
For more information, please visit NXP.com/SE052F.
NXP Semiconductors N.V. (NASDAQ: NXPI) brings together bright minds to create breakthrough technologies that make the connected world better, safer and more secure. As a world leader in secure connectivity solutions for embedded applications, NXP is pushing boundaries in the automotive, industrial & IoT, mobile, and communication infrastructure markets while delivering solutions that advance a more sustainable future. Built on more than 60 years of combined experience and expertise, the company has approximately 34,200 employees in more than 30 countries and posted revenue of $13.28 billion in 2023. Find out more at www.nxp.com.
NXP, EdgeLock and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2024 NXP B.V
View this News Brief in German
Tags: Industrial