Certified to the Bluetooth® 5.3 Low Energy (LE) audio standard, the NXH3675 enables high-quality, multi-stream wireless audio streaming with ultra-low power consumption and latency.
NXP® Semiconductors announced the NXH3675 high-quality audio streaming solution, a highly integrated, single-chip 2.4 GHz transceiver that is certified to the Bluetooth 5.3 LE audio standard. The device enables developers to create innovative products in the Bluetooth audio world with features like high-quality audio transmission, broadcasting capabilities, and multiple audio streams and data channels. With NXP’s optimized audio streaming protocol, the device delivers ultra-low latency with ultra-low power consumption for advanced use cases. Target applications include gaming headsets, hearing aids, soundbars and TV transmitters, and wireless headphones, earbuds, speakers, and microphones.
Bluetooth LE audio has arrived – the next era in Bluetooth audio technology that heralds new and exciting features for an even better user experience. Millions of consumers already use Bluetooth audio devices in everyday life, from earbuds to hearing aids and other hearable devices. According to recent market reports, 1.3 billion Bluetooth audio streaming devices were shipped in 2021, with a forecast of 1.5 billion for 2023. For these applications, the Bluetooth LE audio standard takes audio quality to the next level and brings a new way of experiencing audio. The new standard enables audio sharing, hearing assistance and new use cases that we could not even imagine having with classic Bluetooth audio. NXP has long been at the forefront of Bluetooth audio technology and is currently one of the key players in the most recent Bluetooth 5.3 LE audio standardization.
“The new Bluetooth LE audio standard is set to revolutionize the wireless listening and hearing experience. This requires wireless transceivers with advanced audio processing capabilities that are power efficient with ultra-low latency. The NXH3675 is fully compliant with the new Bluetooth LE audio standard, supporting multiple streams, while having exceptional low power consumption and ultra-low latency.”
Karolien De Baere, Product Marketing and Business Development, NXP Semiconductors
To simplify development and reduce time-to-market, NXP offers the NXH3675 starter kit, which includes an evaluation kit for debug and evaluation purposes, gaming headset and dongle application kits, and a software development kit.
The NXH3675 is sampling now. Learn more about the high-quality audio streaming solution.
NXP Semiconductors N.V. (NASDAQ: NXPI) enables a smarter, safer and more sustainable world through innovation. As a world leader in secure connectivity solutions for embedded applications, NXP is pushing boundaries in the automotive, industrial & IoT, mobile, and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 31,000 employees in more than 30 countries and posted revenue of $11.06 billion in 2021. Find out more at www.nxp.com.
NXP, CoolFlux and the NXP logo are trademarks of NXP B.V. The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc. and any use of such marks by NXP Semiconductors is under license. Arm and Cortex are trademarks or registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere. The related technology may be protected by any or all of patents, copyrights, designs and trade secrets. All rights reserved. All other product or service names are the property of their respective owners. All rights reserved. © 2022 NXP B.V.
Read this News Brief in German