New BTS7202 RX Front End Modules and BTS6403/ 6305 pre-drivers offer higher output power, improved linearity and reduced noise to help improve 5G call quality and internet speed.
NXP® Semiconductors Semiconductors has announced its new higher power BTS7202 RX Front End Modules (FEM) and BTS6403/6305 pre-drivers for 5G massive multiple-input multiple-output (MIMO) going up to 20 W per channel. Developed and implemented in NXP’s silicon germanium (SiGe) process, the devices operate with modest current consumption to reduce operational costs for mobile network operators (MNOs). They also offer improved linearity and reduced noise figure to support better 5G signal quality.
As 5G networks continue to be built out across the globe, MNOs are increasingly leveraging 32T32R solutions to improve massive MIMO coverage in less dense urban and suburban areas. Utilizing 32T32R solutions requires using higher power devices that increase the power level per channel in order to achieve the total power required to ensure strong coverage of the 5G signal.
“With 5G networks beginning to densify, higher power solutions are crucial to ensure network and signal quality remain consistent. Our customers recognize that higher power solutions offer a way for network operators to address the power needs of 32-antenna solutions without compromising network quality.”
Doeco Terpstra, Vice President and General Manager, Smart Antenna Solutions, Radio Power, NXP Semiconductors
The new BTS7202 RX FEMs and BTS6403/6305 pre-drivers offer a comprehensive and easily implemented solution for 5G base stations, complementing NXP’s power amplifier solutions for 32T32R radios. The BTS7202 RX FEMs feature a switch capable of handling up to 20W of power leaking from transmit line-ups, reducing system complexity. The BTS6305 Pre-Drivers also integrate a balun to reduce costs.
For more information, visit NXP’s website .
NXP Semiconductors N.V. (NASDAQ: NXPI) enables a smarter, safer and more sustainable world through innovation. As a world leader in secure connectivity solutions for embedded applications, NXP is pushing boundaries in the automotive, industrial and IoT, mobile, and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 31,000 employees in more than 30 countries and posted revenue of $11.06 billion in 2021. Find out more at www.nxp.com.
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2022 NXP B.V.
Tags: Industrial