AVnu certification fosters an interoperable networking ecosystem and simplifies network synchronization for engineers through AVB and time-synchronized networking (TSN) standards. The certification is aimed at solving major technical and performance issues, including precise timing and real-time synchronization; bandwidth reservation; and traffic shaping, while also minimizing deployment, maintenance and total cost of ownership.
“The increasing number, and complexity of in-vehicle systems is one of the many drivers for AVnu certification to ensure that all parts of an audio-video-bridge system will work together; however, very few companies are capable of executing a certified AVB solution that addresses this interoperability challenge,” said
NXP’s AVB stack includes features such as time-synchronized, low-latency streaming services and bandwidth reservation that makes it possible to carry audio and video signals on a standard Ethernet line. This solves the synchronization challenges between audio and video streaming when video must be displayed on multiple monitors and audio must be harmoniously synchronized across multiple speakers at the same time. The AVnu-certified software provides a complete set of AVB protocols for use on NXP’s i.MX 6 and i.MX 8 applications processors, as well as several other NXP development boards, to reduce the need for hardware changes and eliminating redevelopment costs. It also enables future distributed systems, including NXP’s audio tuners and amplifiers.
In addition to redundant clock master and data traffic capabilities for extreme reliability, key features of NXP’s AVB stack software include precise timing to support low-jitter media clocks, independent traffic classes that enable optimization of network resources, and bounded latency for assurance of timely packet deliveries. The company also provides API to support audio and video applications with the AVB stack.
See NXP Technologies in action at Embedded World 2017 in
Visit NXP during Embedded World in Hall 4A – 220 at the Exhibition Centre Nuremberg. Interact with innovative demonstrations for embedded solutions enabling the IoT from smart cars to smart industry.
For more information about NXP news at Embedded World, please visit www.nxp.com/EW17/mediacenter.
About
NXP and the NXP logo are trademarks of
For more information, please contact:Americas Tate TranTel : +1 408-802-0602Email:tate.tran@nxp.comEurope Martijn van der Linden Tel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China /AsiaEsther Chang Tel: +886 2 8170 9990Email: esther.chang@nxp.com
Tags: Automotive, Industrial