Combined digital instrument cluster and connectivity reference platform delivers high-performance graphics and rich connectivity for an advanced two-wheeler user experience.
NXP® Semiconductors has announced a combined digital instrument cluster and connectivity reference platform designed for mass-market two-wheelers, including motorcycles, electric scooters, commuter bikes and more. The platform combines the high performance i.MX RT1170 crossover MCU with the highly integrated AW611 single-chip Wi-Fi® 6 and Bluetooth®/Bluetooth Low Energy Audio connectivity solution and the KW45 secure wireless access MCU to deliver a highly cost-effective system designed to enhance the user experience of two-wheel mobility. The platform enables high-performance graphics and rich connectivity use cases such as hands-free calling, wireless pairing for smartphone projection, Bluetooth audio, OTA updates, cloud connectivity, fleet management, secure vehicle access and vehicle location.
Two-wheelers have become increasingly electrified, both in the cost-effective vehicles necessary for a daily commute, as well as the higher-end performance vehicles for leisure, with close to 300 million on the roads globally today . Connected digital displays with rich graphics are essential to the safe operation of these EVs, providing critical information that allows drivers to compare navigation details to battery levels and health, as well as the location of charging points. Two-wheeled EVs have a limited range compared with four-wheeled EVs, and these details are essential for safe transit. Telemetry in the field also provides OEMs with important information about usage and battery lifetimes.
NXP’s digital instrument cluster and connectivity reference platform is designed to allow OEMs to deliver these essential capabilities, while also enabling a wide variety of different connectivity use cases designed to improve the user experience. This includes three-way Bluetooth pairing between the phone, scooter’s digital cluster and headphones; rider and pillion music sharing; or even location capabilities such as “find my bike” in a parking lot.
“Whether it’s their daily commute or a leisure trip, drivers look for a cluster that delivers the connectivity features that make their ride more enjoyable and safer. From cluster safety telltales, gauges, phone pairing and music sharing to navigation and electric vehicle charging statistics, NXP's cluster and connectivity reference platform with Vector Graphics enables us to deliver a high-end user experience at a price our OEM customers appreciate.”
Sivakumar Yeddanapudi, Global Senior Director – Cockpit Domain Controller Product Line at Visteon Corporation
“Not only does the digital instrument cluster inform the driver of the state of their vehicle, it also represents the main way a driver can customize their vehicle to their preferences. NXP’s digital instrument cluster and connectivity platform enables consistent updates and customizations to support the latest safety, security and connectivity features, all in a platform that balances performance and wireless connectivity capabilities with cost considerations.”
Dan Loop, Vice President and General Manager, Automotive Edge, NXP
The new cluster and connectivity reference platform leverages NXP’s high performance i.MX RT1170 crossover MCU with AEC-Q100 Grade 3 qualification. This helps reduce system costs due to the highly integrated nature of the i.MX RT1170, which does not require expensive external memory or power management subsystems. The platform comes with NXP Wi-Fi and Bluetooth device drivers pre-integrated into the MCUXpresso SDK, along with display, GNSS and more, making it easy for developers to create their own 2-wheeler connected cluster. The dual-core i.MX RT1170 crossover MCU provides a wide range of interfaces for connecting peripherals, such as WLAN, Bluetooth, GPS, audio, displays and camera sensors, plus a vector graphics accelerator. The i.MX RT1170 crossover MCU’s rich graphics capabilities are supported by NXP’s broad ecosystem of partners, including Altia, The QT Company, Embedded Wizard by TARA Solutions and Crank.
The reference platform also features the AW611, a highly integrated dual-band Wi-Fi 6 and Bluetooth/Bluetooth Low Energy 5.2 single-chip solution with AEC-Q100 Grade 2 qualification. This high degree of integration enables efficient coexistence between internal radios, as well as with external radios, while helping to reduce system costs.
The platform also includes the KW45 BLE wireless MCU to deliver secure vehicle access and vehicle location services. KW45’s three-core architecture integrates a 96 MHz Arm® Cortex®-M33 application core, a dedicated Cortex-M3 radio core and an isolated EdgeLock® secure enclave. It also integrates a Bluetooth Low Energy 5.3-compliant radio that supports up to 24 simultaneous secure connections.
Learn more about Two-Wheeler Connected Digital Clusters.
NXP Semiconductors N.V. (NASDAQ: NXPI) brings together bright minds to create breakthrough technologies that make the connected world better, safer and more secure. As a world leader in secure connectivity solutions for embedded applications, NXP is pushing boundaries in the automotive, industrial & IoT, mobile and communication infrastructure markets while delivering solutions that advance a more sustainable future. Built on more than 60 years of combined experience and expertise, the company has approximately 34,500 team members in more than 30 countries and posted revenue of $13.21 billion in 2022. Find out more at www.nxp.com.
NXP, the NXP logo and EdgeLock are trademarks of NXP B.V. Arm and Cortex are trademarks and/or registered trademarks of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere. The related technology may be protected by any or all of patents, copyrights, designs and trade secrets. All rights reserved. The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG,Inc. and any use of such marks by NXP Semiconductors is under license. All other product or service names are the property of their respective owners. All rights reserved. © 2023 NXP B.V.
View this news brief in German
Tags: Automotive