The SPWM function generates a pulse width modulated waveform in the same way the PWM function does. However, this function facilitates a phase relationship to one or more SPWM channels, allowing a set fixed delay between the transition of the synchronizing channel and the transition of the synchronized channel.
Some of the main features of the SPWM function include:
For more information refer to eTPU General Function Set.