201710043I:SAF7741/SAF7740 Family Marking Introduction Internal Traceabiliy Code DIDT
  • Product Change Notification (PCN)
  • 201710043I

201710043I : SAF7741/SAF7740 Family Marking Introduction Internal Traceabiliy Code DIDT

From 2018 onwards an additional code will be marked on top of the devices from the SAF7741/SAF7740 family to enhance traceabilitiy of the NXP assembly line.This code will be printed on the unused line 5 under the existing device marking and is an unique device ID for traceability purposes only. The unique device ID enables additional traceability of the device production events (man/machine/method/tooling) from WT Assembly to FT for internal process improvements.An example of the new marking is shown in the attached document.

PCN Type Change Category Issue Date Effective Date
Customer Information Notification Product marking 16-Nov-2017 01-Jan-2018

Reason of Change

This change is not expected to affect customers in any way. However because the change is visible NXP wants to appropriately inform customers of it.

Identification of Affected Products

Top side marking Top side marking From 2018 onwards for all products in the SAF7741/SAF7740 family the Marking Line 5 will be used to add an unique device ID for traceability purposes only.

Anticipated Impact

No impact on form fit function reliability or quality.

Affected Parts

Part Number / 12NC Last Time Buy Date Last Time Delivery Date Replacement Part
SAF7741HV/N115ZK
(935302392557)
- - -
SAF7741HV/N115ZY
(935302392518)
- - -
SAF7741HV/N125ZK
(935302418557)
- - -
SAF7741HV/N125ZY
(935302418518)
- - -
SAF7741HV/N135ZK
(935302514557)
- - -
SAF7741HV/N135ZY
(935302514518)
- - -
SAF7741HV/N140ZK
(935302541557)
- - -
SAF7741HV/N140ZY
(935302541518)
- - -