Getting Started with USB-KW40Z | NXP Semiconductors

Getting Started with USB-KW40Z

Last Modified: May 18, 2023Supports USB-KW40Z | KW40Z/30Z/20Z | Wireless

Contents of this document

  • 1

    Plug It In!
  • 2

    Get Software
  • 3

    Run

1. Plug It In!

Let's take your USB-KW40Z for a test drive!

1.1 Attach the USB-KW40Z to the PC

USB-KW40Z-GS-BOARD

USB-KW40Z-GS-BOARD

1.2 Start the board and run the Out-of-Box Demo

Your USB-KW40Z Power green LED should stay ON when you connect the board.

USB-KW40Z-DEMO

USB-KW40Z-DEMO

2. Get Software

In this step, we are going to guide you through the process to get the required software to enable the USB-KW40Z dongle as a Bluetooth Low Energy or IEEE 802.15.4 sniffer. You can also use the USB-KW40Z as a development platform. Select the option you want to accomplish with your USB-KW40Z.

Choose a Development Path:

  • USB-KW40Z Sniffer
  • USB-KW40Z Development Platform

2.1 Download KW40Z Connectivity Software

The KW40Z Connectivity Software package integrates the Kinetis Software Development Kit v1.3 and all the wireless connectivity stacks required to develop your solution using IEEE 802.15.4 and/or Bluetooth Low Energy. It also includes drivers required for the USB-KW40Z.

Click below to download the KW40Z Connectivity Software for your computer.

Get KW40Z Connectivity Software

2.2 Install Wireshark for Bluetooth Low Energy and IEEE 802.15.4 Sniffing

Wireshark is an Open-source network protocol analyzer. It will help you to see what is happening in the wireless communication. It is a great tool for helping to debug issues when talking about wireless connectivity applications.

Get Wireshark network protocol analyze

2.3 Install Kinetis Protocol Analyzer Adapter

In order to enable NXP Wireless Connectivity products, an adapter is needed by wireshark to add support to NXP KW40 device. Please, install this application once you already installed Wireshark.

2.4 Programming USB-KW40Z as Sniffer

USB-KW40Z comes pre-programmed with the sniffer firmware by default. However, if you erased the pre-programmed software in the USB-KW40Z, you can follow the steps provided in the next guide to program USB-KW40Z sniffer application again. Please, click the next button to show you how to program USB-KW40Z with the sniffer firmware.

3. Run

3.1 Configure your Sniffer Tools

USB-KW40Z comes pre-programmed with a sniffer application. Once all the required software is installed in the PC. You are ready to start sniffing your IEEE 802.15.4 or BLE applications. Next buttons provide directions on how to enable your USB-KW40Z on each protocol. Click on the desired protocol to sniff.