Getting Started with the PTN3816EVM Evaluation Board | NXP Semiconductors

Getting Started with the PTN3816EVM Evaluation Board

Last Modified: 2021-06-17 22:51:00

Contents of this document

  • 1

    Out of the Box
  • 2

    Plug It In
  • 3

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the PTN3816EVM evaluation board.

1.1 Kit Contents/Packing List

The PTN3816EVM contents include:

  • Assembled and tested evaluation board in an anti-static bag
  • Quick Start Guide

1.2 Minimum System Requirements

This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.

  • One PC/Notebook with DisplayPort connector
  • One DisplayPort Monitor
  • One micro USB cable to provide power to EVK
  • Two DisplayPort cables (one to be connected between PC and EVK, and the other one to be plugged between EVK and DisplayPort monitor)
  • EVK board

2. Plug It In

2.1 Board Features

  • DisplayPort connections to PC and Monitor
  • Onboard jumper settings for equalizer gain and output swing level

2.2 Board Description

The PTN3816EVM board is designed to be redrive DisplayPort signal outputs from a host graphics card, and to interface with a DisplayPort monitor or a DP-to-HDMI level shifter on the other side. There is a row of DIP switches on the EVM that can change PTN3816’s equalizer, output swing linearity and flat gain settings of redriver channels.

The evaluation board’s power is supplied from a micro-USB connector, and an on-board LDO converts 5.0 V input to both 3.3 V and 1.8 V. 3.3 V is only used to provide power to downstream cable or level shifter dongle. 1.8 V is used for PTN3816.

2.3 Board Components

Overview of the PTN3816EVM evaluation board.

GS-PTN3816EVM-IMG1

GS-PTN3816EVM-IMG1

3. Configure Hardware

3.1 Configure the Hardware

GS-PTN3816EVM-IMG2

GS-PTN3816EVM-IMG2

The PTN3816 evaluation board should be powered with a 5.0 V power supply using a MicroUSB cable (J404). DisplayPort connector on the left side of the board (J401, marked as “TO HOST”) should be connected to a PC’s graphics card through a DisplayPort Cable. DisplayPort connector on the right side of the board (J402, marked as “TO Monitor”) can connect to one of the following for evaluation purposes:

  • DP-2-DP cable → to DisplayPort monitor
  • DP-2-HDMI adapter → to HDMI monitor
  • DP-2-VGA adapter → to VGA monitor