1
Out of the Box2
Get HardwareSign in to save your progress. Don't have an account? Create one.

The NXP analog product development board provides an easy-to-use platform to evaluate NXP products. The board supports a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits (ICs) and system-in-package (SiP) based on proven high-volume technologies. NXP products offer longer battery life, smaller form factors, reduced component counts, lower system cost and improved performance for powering state-of-the-art systems. This page will guide you through the process of setting up and using the EVBMA7318AIO evaluation board (EVB).
The EVBMA7318AIO kit's contents include:
Something went wrong! Please try again.
No additional hardware is required for device evaluation. In addition to the kit contents, the following hardware is beneficial when working with this kit:
Something went wrong! Please try again.
You will need a Windows PC workstation to evaluate the board.
For best results, please use the following operating systems:
Something went wrong! Please try again.
This section covers the EVB components and features.
The EVBMA7318AIO EVB includes the following features:
Something went wrong! Please try again.
The EVBMA7318AIO evaluation board includes two BMA7318 devices controlled by one MCU. Each BMA7318 device measures lithium-ion battery parameters for four to 18 cells. The first BMA7318 communicates with the MCU through isolated SPI and communicates with the second BMA7318 by TPL and transformer isolation. The off-board TPL uses transformer isolation. The MCU is supplied by an SBC that is powered by the 12 VDC power source. Figure 1 below illustrates the board's orientation.
Something went wrong! Please try again.
As shown below, Figure 2 identifies important components on the board. Table 1 (followed by additional tables) provides additional details on these components.
Table 1. Evaluation Board Featured Components Location.
| Number | Devices | Description |
|---|---|---|
| 1 | BMA7318FAIAE | 18-channel lithium-ion battery cell controller (BCC) integrated circuit (IC) with serial peripheral interface-to-transformer physical layer (SPI-to-TPL) communication bridge and current measurement channel |
| 2 | BMA7318TANAE | 18-channel lithium-ion BCC IC with TPL communication and no current measurement channel |
| 3 | FS23 | SBC with CAN physical layer (PHY) and internal power supply for MCU |
| 4 | S32K312 | 32-bit MCU |
Something went wrong! Please try again.
Table 2. J1 JTAG Debug Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | VCC | Power supply for JTAG debugging tool |
| 2 | JTAG_TMS | JTAG test mode selection |
| 3 | GND | Ground |
| 4 | JTAG_TCLK | JTAG test clock |
| 5 | GND | Ground |
| 6 | JTAG_TDO | JTAG data out |
| 7 | NC | Not connected |
| 8 | JTAG_TDI | JTAG data in |
| 9 | GNDDetect | GND detection |
| 10 | JTAG_RSTB | JTAG reset |
Table 3. J1_ High-Voltage Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | NC | Not connected |
| 2 | NC | Not connected |
| 3 | NTC6 | Connect to an external negative temperature coefficient (NTC) thermistor for temperature sensing |
| 4 | NTC5 | Connect to an external NTC thermistor for temperature sensing |
| 5 | NC | Not connected |
| 6 | NC | Not connected |
| 7 | NC | Not connected |
| 8 | NC | Not connected |
| 9 | GND | Ground of BCC |
| 10 | C1P | Cell 1 voltage sensing point |
| 11 | C3P | Cell 3 voltage sensing point |
| 12 | C5P | Cell 5 voltage sensing point |
| 13 | C6Pb | Cell 6 voltage sensing point b |
| 14 | C8P | Cell 8 voltage sensing point |
| 15 | C10P | Cell 10 voltage sensing point |
| 16 | C12Pa | Cell 12 voltage sensing point b |
| 17 | C13P | Cell 13 voltage sensing point |
| 18 | C15P | Cell 15 voltage sensing point |
| 19 | C17P | Cell 17 voltage sensing point |
| 20 | VPWR | Power supply for the BCC |
| 21 | NC | Not connected |
| 22 | NC | Not connected |
| 23 | NC | Not connected |
| 24 | GND | Ground of NTC thermistors |
| 25 | GND | Ground of NTC thermistors |
| 26 | GND | Ground of NTC thermistors |
| 27 | GND | Ground of NTC thermistors |
| 28 | GND | Ground of NTC thermistors |
| 29 | GND | Ground of NTC thermistors |
| 30 | C0M | Cell 0 voltage sensing point |
| 31 | C2P | Cell 2 voltage sensing point |
| 32 | C4P | Cell 4 voltage sensing point |
| 33 | C6Pa | Cell 6 voltage sensing point a |
| 34 | C7P | Cell 7 voltage sensing point |
| 35 | C9P | Cell 9 voltage sensing point |
| 36 | C11P | Cell 11 voltage sensing point |
| 37 | C12Pb | Cell 12 voltage sensing point b |
| 38 | C14P | Cell 14 voltage sensing point |
| 39 | C16P | Cell 16 voltage sensing point |
| 40 | C18P | Cell 18 voltage sensing point |
Table 4. J1_2 High-Voltage Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | AIN10 | Should connect to an external NTC thermistor for temperature sensing |
| 2 | NTC7 | Connect to external NTC thermistors for temperature sensing |
| 3 | NTC6 | Connect to external NTC thermistors for temperature sensing |
| 4 | NTC5 |
Connect to external NTC thermistors for temperature sensing |
| 5 | NTC4 |
Connect to external NTC thermistors for temperature sensing |
| 6 | NTC3 |
Connect to external NTC thermistors for temperature sensing |
| 7 | NTC2 |
Connect to external NTC thermistors for temperature sensing |
| 8 | NTC1 |
Connect to external NTC thermistors for temperature sensing |
| 9 | GND | Ground for BCC |
| 10 | C1P | Cell 1 voltage sensing point |
| 11 | C3P | Cell 3 voltage sensing point |
| 12 | C5P | Cell 5 voltage sensing point |
| 13 | C6Pb | Cell 6 voltage sensing point b |
| 14 | C8P | Cell 8 voltage sensing point |
| 15 | C10P | Cell 10 voltage sensing point |
| 16 | C12Pa | Cell 12 voltage sensing point b |
| 17 | C13P | Cell 13 voltage sensing point |
| 18 | C15P | Cell 15 voltage sensing point |
| 19 | C17P | Cell 17 voltage sensing point |
| 20 | VPWR | Power supply for the BCC |
| 21 | AIN11 | Should connect to an external NTC thermistor for temperature sensing |
| 22 | NTC8 | Connect to external NTC thermistors for temperature sensing |
| 23 | NTC9 | Connect to external NTC thermistors for temperature sensing |
| 24 | GND |
Ground for NTC thermistors |
| 25 | GND |
Ground for NTC thermistors |
| 26 | GND |
Ground for NTC thermistors |
| 27 | GND |
Ground for NTC thermistors |
| 28 | GND |
Ground for NTC thermistors |
| 29 | GND |
Ground for NTC thermistors |
| 30 | C0M | Cell 0 voltage sensing point |
| 31 | C2P | Cell 2 voltage sensing point |
| 32 | C4P | Cell 4 voltage sensing point |
| 33 | C6Pa | Cell 6 voltage sensing point a |
| 34 | C7P | Cell 7 voltage sensing point |
| 35 | C9P | Cell 9 voltage sensing point |
| 36 | C11P | Cell 11 voltage sensing point |
| 37 | C12Pb | Cell 12 voltage sensing point b |
| 38 | C14P | Cell 14 voltage sensing point |
| 39 | C16P | Cell 16 voltage sensing point |
| 40 | C18P | Cell 18 voltage sensing point |
Table 5. J2_2 TPL Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | B2-H_INOUT+ | Positive of TPL_H twisted wire on BMA7318TANAE |
| 2 | B2-H_INOUT- | Negative of TPL_H twisted wire on BMA7318TANAE |
Table 6. J3 Low-Voltage Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | FS23_CANL | CAN bus negative (low) |
| 2 | FS23_CANH | CAN bus positive (high) |
| 3 | VBAT | 12 VDC power supply for the MCU |
| 4 | VBAT | 12 VDC power supply for the MCU |
| 5 | NC | Not connected |
| 6 | NC | Not connected |
| 7 | KL15_WKP | Wake-up source from KL15 |
| 8 | GND | MCU ground |
Table 7. J4_1 SHUNT Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | B1-GND | Ground of BMA7318FAIAE |
| 2 | B1-ISENSE- | Current measurement wire is negative |
| 3 | B1-ISENSE+ | Current measurement wire is positive |
| 4 | B1-NTC-SHUNT | Temperature monitoring NTC for shunt |
Table 8. J5_1 High-Voltage Point Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | PACK+ | PACK+ high-voltage measurement point |
| 2 | NC | Not connected |
| 3 | LINK+ | LINK+ high-voltage measurement point |
| 4 | NC | Not connected |
| 5 | LINK- | LINK- high-voltage measurement point |
Table 9. JP1 External SPI Interface Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | VDD_MCU | Power supply from MCU |
| 2 | GND | MCU ground |
| 3 | EXT_CSB | SPI chip select input from an external device |
| 4 | EXT_SCLK | SPI clock input from an external device |
| 5 | EXT_MOSI | SPI controller output, target input from an external device |
| 6 | EXT_MISO | SPI controller input, target output to an external device |
| 7 | NC | Not connected |
| 8 | NC | Not connected |
Table 10. JP2 External UART Interface Connector Description.
| Pin | Name | Description |
|---|---|---|
| 1 | NC | Not connected |
| 2 | NC | Not connected |
| 3 | UART_RX_S32K | UART receive wire (signal) for the S32K312 |
| 4 | UART_TX_S32K | UART transmit wire (signal) for the S32K312 |
| 5 | GND | GND: MCU ground |
| 6 | VDD_MCU | Power supply from MCU |
Something went wrong! Please try again.