Sign in for a personalized NXP experience.
1
Solution Hardware2
Get to Know the Software3
Unbox and Setup4
Assembly5
Plug it InSign in to save your progress. Don't have an account? Create one.
Get the required hardware and miscellaneous hardware and tools
The EasyEVSE EV Charging Development Platform (FreeRTOS, Wi-Fi 4) with ISO 15118-2 implementation requires an Electric Vehicle Supply Equipment (EVSE) and an Electric Vehicle (EV) side, with related hardware, software and miscellaneous hardware, to run the setup.
The hardware required to assemble, wire, and run the EasyEVSE is listed below:
For the EVSE side:
For the EV side:
By using Wi-Fi connectivity:
Something went wrong! Please try again.
The miscellaneous hardware and tools required to assembly the platform is shown below:
Optional, if the Wi-Fi is to be connected additional miscellaneous hardware and tools are required:
NOTE: If using the Wi-Fi only, there is no need for soldering iron and solder core wire, ESD tweezers and RJ45 Ethernet UTP cable
Something went wrong! Please try again.
Get the required software
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This short video list all the required software for this initial simplified setup.
The below sections provide links to the required software.
Download and install the latest version of the IDE for your operating system.
Something went wrong! Please try again.
Build, download and install the MCUXpresso SDK for your MIMXRT1060-EVKB or MIMXRT1064-EVK and TWR-KM3x board variant.
Something went wrong! Please try again.
The EasyEVSE Development Platform (FreeRTOS, Wi-Fi 4) has an EVSE and an EV software part. The software for the EV and EVSE side comes in one zip file.
Download the software for your used RT106x EVK: Releases · nxp-appcodehub/rd-nxp-easyevse-imxrt106x
In addition, also download the software for the EasyEVSE EV charging signal board (EVSE-SIG-BRD1X/2X). Here are two software packages to download, one software for the EVSE and one software for the EV side.
EVSE-SIG-BRD1X/2X software for the for the EVSE side: Releases · nxp-appcodehub/dm-lpc5536-evse-sigbrd
EVSE-SIG-BRD1X/2X software for the for the EV side: Releases · nxp-appcodehub/dm-evse-sigbrd1x-ev-software-on-lpc5536
Something went wrong! Please try again.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This video describes the unboxing and setup of each one of the EasyEVSE development boards and LCD. Including the creation and setup of Azure IoT Central application, using a shareable link template and the configuration of a mutually secure and authenticated connection with the Azure IoT Central.
The communication with the server is done over the Ethernet.
Something went wrong! Please try again.
This chapter shows how to assembly all the components which are part of the development platform.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This video shows the steps to stack and connect all the boards of the platform.
Something went wrong! Please try again.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
The video shows how to connect the EasyEVSE EV charging signal board (EVSE-SIG-BRD1X/2X), the metering board (TWR-KM35Z75M or TWR-KM34Z75M, or TWR-KM34Z50M), Wi-Fi (with the 1XK M.2 Module together with the LBEE0ZZ1WE-uSD-M2), the NFC board (CLEV6630ARD) and secure element board (OM-SE050ARD-E) with the host controller bord (MIMXRT1060-EVK/MIMXRT1060-EVKB/MIMXRT1060-EVKC or MIMXRT1064-EVK). Check the User Guide to know how to connect the touch display to your host controller board.
Something went wrong! Please try again.
This chapter show cases the EasyEVSE Development Platform (FreeRTOS, Wi-Fi 4) with ISO 15118-2 implementation.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This video shows how the solutions works after successfully enabled the development platform, including required software settings, driving the ISO 15118-2 stack between the EVSE and EV side, cloud connection and the graphical user interface (GUI), presenting on the touch display.
Once you successfully completed this getting started setup, refer to the available design resources.
The User Guide provides additional information on how to use your Azure IoT Central application to monitor telemetry, update properties and send commands to your EasyEVSE device.
To simplify the start-up process, the Plug and Trust SE050 secure element was not implemented in this Getting Started setup. Refer to the User Manual to learn how to implement it and to get a detailed description of each building block of the platform.
Something went wrong! Please try again.