AC Induction Motors | ||
![]() |
The stator windings of an AC induction motor are distributed around the stator to produce a roughly sinusoidal distribution. When three phase ac voltages are applied to the stator windings, a rotating magnetic field is produced. The rotor of an induction motor also consists of windings or more often a copper squirrel cage imbeded within iron laminates. Only the iron laminates are shown. An electric current is induced in the rotor bars which also produce a magnetic field. The rotating magnetic field of the stator drags the rotor around. The rotor does not quite keep up with the the rotating magnetic field of the stator. It falls behind or slips as the field rotates. In this animation, for every time the magnetic field rotates, the rotor only makes three forths of a turn. If you follow one of the bright green or red rotor teeth with the mouse, you will notice it change color as it falls behind the rotating field. The slip has been greatly exagerated to enable visualization of this concept. A real induction motor only slips a few percent. |
|