NXP® Semiconductors | MSE9S12XS256_0M05M |
Mask Set Errata | Rev. April 16, 2012 |
MC9S12XS256, Mask 0M05M |
This errata sheet applies to the following devices: MC9S12XS256 |
The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code. |
Device markings indicate the week of manufacture and the mask set used. The date is coded as four
numerical digits where the first two digits indicate the year and the last two digits indicate the work week.
For instance, the date code "0201" indicates the first week of the year 2002. |
Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix. |
MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum. |
Errata Number | Module affected | Brief Description | Work- around |
MUCts03867 | s12_cpu_xs | CPU: Breakpoint missed at simultaneous taghits | YES |
MUCts03977 | pwm_8b8c | PWM: Emergency shutdown input can be overruled | YES |
MUCts04135 | pwm_8b8c | PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | YES |
MUCts04136 | pwm_8b8c | PWM: Wrong output value after restart from stop or wait mode | YES |
MUCts04157 | tim_16b8c | TIM_16B8C: Output compare pulse is inaccurate | YES |
MUCts04177 | s12xe_crg | s12xe_crg: Possible PLL premature LOCK followed by an UN-LOCK in conjunction with STOP instruction | YES |
MUCts04243 | sci | SCI: RXEDGIF occurs more times than expected in IR mode | YES |
CPU: Breakpoint missed at simultaneous taghits | MUCts03867 |
The CPU execution priority encoder evaluates taghits and then |
Do not attach multiple tags to the same exact address. |
PWM: Emergency shutdown input can be overruled | MUCts03977 |
If the PWM emergency shutdown feature is enabled (PWM7ENA=1) and PWM |
When using the PWM emergency shutdown feature the GPIO function on the |
PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | MUCts04135 |
When the PWM is used in 16-bit (concatenation) channel and the emergency |
If emergency shutdown mode is required: |
PWM: Wrong output value after restart from stop or wait mode | MUCts04136 |
In low power modes (P-STOP/STOP/WAIT mode) and during PWM7 |
Before entering low power modes, user can disable the related PWM |
TIM_16B8C: Output compare pulse is inaccurate | MUCts04157 |
The pulse width of an output compare (which resets the free running |
The specification has been updated. Please refer to revision V02.07 (04 |
s12xe_crg: Possible PLL premature LOCK followed by an UN-LOCK in conjunction with STOP instruction | MUCts04177 |
If the PLL is manually turned off (PLLCTL_ PLLON = 0) before a STOP |
Do not modify the PLLON bit around the STOP instruction. |
SCI: RXEDGIF occurs more times than expected in IR mode | MUCts04243 |
Configured for Infrared Receive mode, the SCI may incorrectly set the |
Case 1 and case 2 may occurs at same time. To avoid those unexpected |