NXP® Semiconductors | MSE9S12XHZ512_1M80F |
Mask Set Errata | Rev. April 17, 2012 |
MC9S12XHZ512, Mask 1M80F |
This errata sheet applies to the following devices: MC9S12XHZ512 |
The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code. |
Device markings indicate the week of manufacture and the mask set used. The date is coded as four
numerical digits where the first two digits indicate the year and the last two digits indicate the work week.
For instance, the date code "0201" indicates the first week of the year 2002. |
Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix. |
MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum. |
Errata Number | Module affected | Brief Description | Work- around |
MUCts03390 | atd_10b16c | ATD: Abort of an A/D conversion sequence with write to ATDxCTL0/1/2/3 may not work | YES |
MUCts03439 | iic | IIC: 10-bit Slave is misaddressed by the data | YES |
MUCts03446 | iic | IIC:10-Bit Slave fails to acknowledge address on a second transfer | YES |
MUCts03447 | iic | IIC:10-bit Master addresses itself by a faulty acknowledge | NO |
MUCts03449 | iic | IIC: 10-bit Slave does not acknowledge address if the last data is $XF | YES |
MUCts03564 | mscan | MSCAN: Corrupt ID may be sent in early-SOF condition | YES |
MUCts03641 | s12x_dbg | DBG in Pure PC mode - too many trace buffer entries generated | NO |
MUCts03642 | s12x_dbg | DBG No address match if next transaction is misaligned word access | YES |
MUCts03649 | eetx_4k | eetx4k An interrupt following immediately after execution of a STOP instruction may disable read access to the EEPROM array | YES |
MUCts03653 | vreg_3v3 | vreg_3v3.05.02: Possible incorrect operation if device is wakened from stop mode within 4.7µs of stop mode entry | NO |
MUCts03689 | atd_10b16c | ADC: conversion does not start with 2 consecutive writes to ATDCTL5 | YES |
MUCts03760 | s12x_dbg | DBG: State flags and counter corrupted by simultaneous arm and disarm | YES |
MUCts03871 | s12x_cpu | CPU: Breakpoint missed at simultaneous taghits | YES |
MUCts03977 | pwm_8b8c | PWM: Emergency shutdown input can be overruled | YES |
MUCts04086 | pim_9xhz512 | PIM: Edge-sensitive mode of IRQ-pin may cause incorrect interrupt vector fetch | YES |
MUCts04104 | ect_16b8c | ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1 | YES |
MUCts04135 | pwm_8b8c | PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | YES |
MUCts04136 | pwm_8b8c | PWM: Wrong output value after restart from stop or wait mode | YES |
MUCts04156 | ect_16b8c | ECT_16B8C: Output compare pulse is inaccurate | YES |
MUCts04166 | ftx_512k4 | Flash: Burst programming issue if bus clock frequency is higher than oscillator clock frequency | YES |
MUCts04238 | ftx_512k4 | FTX: Flash Command influenced by Backdoor Key write | YES |
MUCts04244 | sci | SCI: RXEDGIF occurs more times than expected in IR mode | YES |
ATD: Abort of an A/D conversion sequence with write to ATDxCTL0/1/2/3 may not work | MUCts03390 |
Starting a conversion with a write to ATDxCTL5 or on an external trigger |
Only write to ATDxCTL4 to abort an ongoing conversion sequence. |
IIC: 10-bit Slave is misaddressed by the data | MUCts03439 |
10-bit Master-Transmitter, Slave-Receiver transfer - The Slave fails |
Avoid using a first data byte value that is the same as the third |
IIC:10-Bit Slave fails to acknowledge address on a second transfer | MUCts03446 |
10-bit Master-Receiver, Slave-Transmitter transfer - When a part is |
When configuring the IIC as a Receiver (Tx/Rx = 0), first disable the |
IIC:10-bit Master addresses itself by a faulty acknowledge | MUCts03447 |
10-bit Master-Transmitter, Slave-Receiver transfer - The Master does |
None. |
IIC: 10-bit Slave does not acknowledge address if the last data is $XF | MUCts03449 |
10-Bit Master-Receiver, Slave-Transmitter transfer - The Slave fails |
Avoid using last data bytes in transfers in the range 0xXF; where |
MSCAN: Corrupt ID may be sent in early-SOF condition | MUCts03564 |
The initial eight ID bits will be corrupted if a message is set up for |
Due to increased oscillator tolerance a transmission start in the third |
DBG in Pure PC mode - too many trace buffer entries generated | MUCts03641 |
If configured for Pure PC mode tracing, an extra, unexpected trace |
None. |
DBG No address match if next transaction is misaligned word access | MUCts03642 |
Memory accesses in successive bus cycles must both be able to generate |
Insert a NOP instruction before misaligned word accesses if they can |
eetx4k An interrupt following immediately after execution of a STOP instruction may disable read access to the EEPROM array | MUCts03649 |
An interrupt request immediately following execution of a STOP |
If the STOP instruction is executed while interrupts are enabled, read |
vreg_3v3.05.02: Possible incorrect operation if device is wakened from stop mode within 4.7µs of stop mode entry | MUCts03653 |
It is possible that after the device enters Stop or Pseudo-Stop mode it |
None. |
ADC: conversion does not start with 2 consecutive writes to ATDCTL5 | MUCts03689 |
When the ATD is started with write to ATDCTL5 |
Only write once to ATDCTL5 when starting a conversion. |
DBG: State flags and counter corrupted by simultaneous arm and disarm | MUCts03760 |
Simultaneous disarming (hardware) and arming (software) results in |
If the fault condition is caused by writing to DBGC1 to set the TRIG |
CPU: Breakpoint missed at simultaneous taghits | MUCts03871 |
The CPU execution priority encoder evaluates taghits and then |
Do not attach multiple tags to the same exact address. |
PWM: Emergency shutdown input can be overruled | MUCts03977 |
If the PWM emergency shutdown feature is enabled (PWM7ENA=1) and PWM |
When using the PWM emergency shutdown feature the GPIO function on the |
PIM: Edge-sensitive mode of IRQ-pin may cause incorrect interrupt vector fetch | MUCts04086 |
Where the IRQ interrupt is being used in edge-sensitive mode and a |
Where using IRQ in edge-sensitive mode then configure the interrupt |
ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1 | MUCts04104 |
Channel 0 – 3 Input Capture interrupts are inhibited when BUFEN=1, |
A simple workaround exists for this errata: |
PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | MUCts04135 |
When the PWM is used in 16-bit (concatenation) channel and the emergency |
If emergency shutdown mode is required: |
PWM: Wrong output value after restart from stop or wait mode | MUCts04136 |
In low power modes (P-STOP/STOP/WAIT mode) and during PWM7 |
Before entering low power modes, user can disable the related PWM |
ECT_16B8C: Output compare pulse is inaccurate | MUCts04156 |
The pulse width of an output compare (which resets the free running |
The specification has been updated. Please refer to revision V03.08 (04 |
Flash: Burst programming issue if bus clock frequency is higher than oscillator clock frequency | MUCts04166 |
If S12X is running at a bus clock frequency higher than the oscillator |
Adding a time delay between the check of CBEIF flag and the start of the |
FTX: Flash Command influenced by Backdoor Key write | MUCts04238 |
When executing a flash erase verify (0x05) command sequence to a flash |
Write 0x30 to FSTAT register (ACCERR = 1, PVIOL = 1) prior to |
SCI: RXEDGIF occurs more times than expected in IR mode | MUCts04244 |
Configured for Infrared Receive mode, the SCI may incorrectly set the |
Case 1 and case 2 may occurs at same time. To avoid those unexpected |