Freescale Semiconductor | MSE9S12XF512_1M64J |
Mask Set Errata | Rev. April 16, 2012 |
MC9S12XF512, Mask 1M64J |
This errata sheet applies to the following devices: MC9S12XF512, MC9S12XF384, MC9S12XF256, MC9S12XF128 |
The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code. |
Device markings indicate the week of manufacture and the mask set used. The date is coded as four
numerical digits where the first two digits indicate the year and the last two digits indicate the work week.
For instance, the date code "0201" indicates the first week of the year 2002. |
Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix. |
MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum. |
Errata Number | Module affected | Brief Description | Work- around |
MUCts03731 | s12x_dbg | DBG: State flags and counter corrupted by simultaneous arm and disarm | YES |
MUCts03765 | ftm_512k3 | FTM: ECC faults not detected at the end of an erase verify range | YES |
MUCts03796 | adc_12b16c | ADC: converting value (Vrefh-Vrefl)/4 could give wrong result | YES |
MUCts03821 | ftm_512k3 | FTM: EEPROM Emulation corruption on consecutive resets | YES |
MUCts03822 | ftm_512k3 | FTM: EEPROM Emulation Erroneous Dead Sectors | NO |
MUCts03823 | ftm_512k3 | FTM: EEPROM Emulation corruption on consecutive Enable EEPROM Emulation Commands | YES |
MUCts03859 | mcu_9s12xf512 | FTM: Version ID qualifier for FTM errata | NO |
MUCts03867 | s12_cpu_xs | CPU: Breakpoint missed at simultaneous taghits | YES |
MUCts03934 | s12x_bdm | BDM: Incomplete Memory Access on misaligned access due to BDM features | YES |
MUCts03987 | ftm_512k3 | FTM: EEE Brownout handling | YES |
MUCts04085 | s12xf512_pim | PIM: Edge-sensitive mode of IRQ-pin may cause incorrect interrupt vector fetch | YES |
MUCts04104 | ect_16b8c | ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1 | YES |
MUCts04156 | ect_16b8c | ECT_16B8C: Output compare pulse is inaccurate | YES |
MUCts04177 | s12xe_crg | s12xe_crg: Possible PLL premature LOCK followed by an UN-LOCK in conjunction with STOP instruction | YES |
MUCts04244 | sci | SCI: RXEDGIF occurs more times than expected in IR mode | YES |
DBG: State flags and counter corrupted by simultaneous arm and disarm | MUCts03731 |
Simultaneous disarming (hardware) and arming (software) results in |
If the fault condition is caused by writing to DBGC1 to set the TRIG |
FTM: ECC faults not detected at the end of an erase verify range | MUCts03765 |
The memory controller can prematurely halt an erase verify in the case |
Any ECC faults in skipped locations will be detected and flagged during |
ADC: converting value (Vrefh-Vrefl)/4 could give wrong result | MUCts03796 |
When the Analogue to Digital Converter converts an analogue value of |
It is not possible to avoid the error occurring, however, it is possible |
FTM: EEPROM Emulation corruption on consecutive resets | MUCts03821 |
If the EEPROM Emulation flow is reset (or powered down) during the |
Ensuring the following will minimize susceptibility to this scenario - |
FTM: EEPROM Emulation Erroneous Dead Sectors | MUCts03822 |
If the EEPROM Emulation flow is reset (or powered down) within a 20us |
Ensuring the following will minimize susceptibility to this scenario - |
FTM: EEPROM Emulation corruption on consecutive Enable EEPROM Emulation Commands | MUCts03823 |
If the EEPROM Emulation flow is reset (or powered down) during a data |
Only execute the Enable Emulated EEPROM command once in the application |
FTM: Version ID qualifier for FTM errata | MUCts03859 |
This entry provides information with regard to patches applied in |
N/A |
CPU: Breakpoint missed at simultaneous taghits | MUCts03867 |
The CPU execution priority encoder evaluates taghits and then |
Do not attach multiple tags to the same exact address. |
BDM: Incomplete Memory Access on misaligned access due to BDM features | MUCts03934 |
If a misaligned word write access is directly followed by an attempted |
Do not set breakpoints or insert BGND after a GSTD. |
FTM: EEE Brownout handling | MUCts03987 |
There is an issue in the case of a reset occurring at specific |
While it is not possible to avoid the error occurring, it is possible |
PIM: Edge-sensitive mode of IRQ-pin may cause incorrect interrupt vector fetch | MUCts04085 |
Where the IRQ interrupt is being used in edge-sensitive mode and a |
Where using IRQ in edge-sensitive mode then configure the interrupt |
ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1 | MUCts04104 |
Channel 0 – 3 Input Capture interrupts are inhibited when BUFEN=1, |
A simple workaround exists for this errata: |
ECT_16B8C: Output compare pulse is inaccurate | MUCts04156 |
The pulse width of an output compare (which resets the free running |
The specification has been updated. Please refer to revision V03.08 (04 |
s12xe_crg: Possible PLL premature LOCK followed by an UN-LOCK in conjunction with STOP instruction | MUCts04177 |
If the PLL is manually turned off (PLLCTL_ PLLON = 0) before a STOP |
Do not modify the PLLON bit around the STOP instruction. |
SCI: RXEDGIF occurs more times than expected in IR mode | MUCts04244 |
Configured for Infrared Receive mode, the SCI may incorrectly set the |
Case 1 and case 2 may occurs at same time. To avoid those unexpected |