NXP® SemiconductorsMSE9S12UF32_1L79R
Mask Set ErrataRev. April 17, 2012



MC9S12UF32, Mask 1L79R


Introduction
This errata sheet applies to the following devices:

MC9S12UF32



MCU Device Mask Set Identification

The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code.



MCU Device Date Codes

Device markings indicate the week of manufacture and the mask set used. The date is coded as four numerical digits where the first two digits indicate the year and the last two digits indicate the work week. For instance, the date code "0201" indicates the first week of the year 2002.



MCU Device Part Number Prefixes

Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix.



Errata System Tracking Numbers

MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum.



Errata Summary


Errata NumberModule affectedBrief DescriptionWork-
around
MUCts00755 S12_bdm BDM: ACK conflict exiting STOP YES
MUCts00762 S12_cpu DBG: CPU erroneously causes BSRs to be recorded in trace buffer YES
MUCts01008 fts32k Array writes immediately after FPROT write do not set PVIOL flag. YES
MUCts01050 fts32k Flash: ACCERR is not set for a Byte Access YES
MUCts01051 fts32k STOP instruction may not set ACCERR flag NO
MUCts01966 S12_bdm Possible manipulation of return address when exiting BDM active mode YES
MUCts02415 S12_mebi MEBI: Missing ECLK edge on first external access after mode switching YES
MUCts04159 tim_16b8c TIM:Normal Output Compare event happens on setting OC7M bit if OM/OL=0 YES
MUCts04161 tim_16b8c TIM_16B8C: Output compare pulse is inaccurate YES
MUCts04248 sci SCI: RXEDGIF occurs more times than expected in IR mode YES



BDM: ACK conflict exiting STOPMUCts00755

Description

When using the Background Debugger to debug 

code which contains STOP instructions, the
host debugger can lose clock sync with the
target device. If the ACK protocol is enabled,
a target command which is expecting to send
and ACK pulse, can conflict with a host issued
SYNC command attempting to re-establish clock
sync between the host and target.

Workaround


The ACK protocol can be disabled when debugging

source code which contains STOP instructions.
The host SYNC command may then be used to re-establish
clock sync between the host and target after
a STOP instruction.



DBG: CPU erroneously causes BSRs to be recorded in trace bufferMUCts00762

Description

The BSR instruction is recognized as a change of flow instruction and

thus causes the trace buffer to be loaded with its destination address.
Since the BSR instruction always branches to the relative address
specified in the instruction, the information stored in the trace buffer
at a BSR is not useful. Thus code making regular use of the BSR
instruction will result in considerable redundancy in trace buffer
contents.


Workaround


The severity of this bug is directly related to the frequency of BSR 

instruction use. Thus to reduce the impact of this bug, use of the BSR
instruction should be avoided wherever possible.





Array writes immediately after FPROT write do not set PVIOL flag.MUCts01008

Description

A write to the flash protection register that is immediately followed by

a flash array write will not set the PVIOL protection violation flag.

Example:
MOVB #$FB FPROT //protect lower portion of flash page $3E
STD #$55AA #$8080 //write to protected address (PVIOL flag expected,
but does not occur)

Workaround


Perform a legal write of a register immediately after writing to the

FPROT register, before writing to the flash array.

Example:
MOVB #$FB FPROT //protect lower portion of flash page $3E
MOVB #$30 FSTAT //clear error flags (legal write to register)
STD #$55AA #$8080 //write to protected address (PVIOL flag sets to show
protection violation)



Flash: ACCERR is not set for a Byte AccessMUCts01050

Description

Starting a command sequence with a MOVB array write instruction (Byte

Write) will not generate an access error. The command is processed
normally programming the array according to the content (word) of the
data register while only the high byte in the FDATA register holds valid
information.

Workaround


Avoid the use of MOVB instruction for array program operations.  




STOP instruction may not set ACCERR flagMUCts01051

Description

If a STOP instruction is issued between the time when an NVM command is

completed and the time when the NVM CCIF command complete flag is set,
the ACCERR flag will not be set.

Workaround


None.



Possible manipulation of return address when exiting BDM active modeMUCts01966

Description

Upon leaving BDM active mode, the CPU return address is stored

temporarily for a few cycles in the BDM shift register. If a BDM command
transmission is detected during this time, the return address will be
manipulated in the BDM shift register. This situation is likely to occur
when a CPU BGND instruction is executed in user code during debugging
under the following conditions:

(i) The BDM module is not enabled AND
(ii) BDM commands are sent from the host

If this situation occurs, the CPU will execute BDM firmware and will
check the status of the ENBDM bit in the BDMSTS register. If the BDM is
disabled, the ENBDM bit will be clear, and hence the BDM firmware will
be exited and the shift register manipulation described above will occur.

Workaround


Avoid using the BGND instruction when the ENBDM bit in the BDMSTS

register is cleared.



MEBI: Missing ECLK edge on first external access after mode switchingMUCts02415

Description

If the ECLK is used as an external bus control signal (ESTR=1) the first

external access is lost after switching from a single chip mode with
enabled ECLK output to an expanded mode. The ECLK is erroneously held in
the high phase thus the first external bus access does not generate a
rising ECLK edge for the external logic to latch the address. The ECLK
stretches low after the lost access resulting in all following external
accesses to be valid.

Workaround


Enter expanded mode with ECLK output disabled (NECLK=1). Enable the ECLK

after switching the mode before executing the first external access.



TIM:Normal Output Compare event happens on setting OC7M bit if OM/OL=0 MUCts04159

Description

When an OC7M bit is set, an erroneous normal output compare event can 

happen on a timer port if the compare action is selected as "Timer
disconnected from output pin logic ".

Corresponding configuration:
* TIOSx = 1 --> Output compare mode
* OMx = OLx = 0 --> Output compare logic disconnected from the pin
* OC7Mx = 1 --> Mask bit set for OC7 event







Workaround


Set OC7Mx = 1 only for channels where the output compare action should 

drive the pin, and OC7Mx = 0 for all other channels where the pin is
required to be disconnected from the output compare logic.



TIM_16B8C: Output compare pulse is inaccurateMUCts04161

Description

The pulse width of an output compare (which resets the free running

counter when TCRE = 1) will measure one more bus clock cycle than
expected.



Workaround


The specification has been updated. Please refer to revision 01.09 (07

May 2010) or later.

In description of bitfield TCRE in register TSCR2,a note has been added:
TCRE=1 and TC7!=0, the TCNT cycle period will be TC7 x "prescaler
counter width" + "1 Bus Clock". When TCRE is set and TC7 is not equal to
0, then TCNT will cycle from 0 to TC7. When TCNT reaches TC7 value, it
will last only one bus cycle then reset to 0.









SCI: RXEDGIF occurs more times than expected in IR modeMUCts04248

Description

Configured for Infrared Receive mode, the SCI may incorrectly set the 

RXEDGIF bit if there are consecutive '00' data bits. There are two
cases:

Case 1: due to re-sync of the RXD input, the received edge may be
delayed by one bus cycle. If an edge (bit = '0') is detected near
an SCI clock edge, the next edge (bit = '0') may be detected one
SCI clock later than expected due to re-sync logic.

Case 2: if external baud is slower than SCI receiver, the next edge
may be detected later than expected.

This glitch can be detected by the RXEDGIF circuit, but it does not
impact the final data result because the SCI receive and data recovery
logic takes samples at RT8, RT9, and RT10.




Workaround


Case 1 and case 2 may occurs at same time. To avoid those unexpected 

RXEDGIF at IR mode, the external baud should be kept a little bit
faster than receiver baud by:
P > (1/16)/(SBR)
or
(P)(SBR)(16)> 1

Where SBR is baud of receiver, P is external baud faster ratio.
For example:
1.- When SBR = 16, P = 0.4%, this means the external baud should be at
least 0.4% faster than receiver.
2.- When SBR = 4, P = 1.6%, this means the external baud should be at
least 1.6% faster than receiver.

Case 1 will cover case 2, i.e. case 1 is the worst case. If case1 is
solved, case 2 is also solved.


© NXP Semiconductors, Inc., 2012. All rights reserved.