NXP® Semiconductors | MSE9S12HY64_0M34S |
Mask Set Errata | Rev. April 16, 2012 |
MC9S12HY64, Mask 0M34S |
This errata sheet applies to the following devices: MC9S12HY64, MC9S12HA64 |
The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code. |
Device markings indicate the week of manufacture and the mask set used. The date is coded as four
numerical digits where the first two digits indicate the year and the last two digits indicate the work week.
For instance, the date code "0201" indicates the first week of the year 2002. |
Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix. |
MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum. |
Errata Number | Module affected | Brief Description | Work- around |
MUCts04089 | s12_cpmu | API interrupt flag sets unexpectedly upon entering STOP mode | YES |
MUCts04157 | tim_16b8c | TIM_16B8C: Output compare pulse is inaccurate | YES |
MUCts04170 | s12_cpmu | CPMU: High probabilty of PLL Loss of LOCK and UPOSC status change when using Adaptive Oscillator Filter with OSCBW=0 and high VCOCLK frequency | YES |
MUCts04202 | pwm_8b8c | PWM: Wrong output value after restart from stop or wait mode | YES |
MUCts04205 | pwm_8b8c | PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | YES |
MUCts04243 | sci | SCI: RXEDGIF occurs more times than expected in IR mode | YES |
API interrupt flag sets unexpectedly upon entering STOP mode | MUCts04089 |
The problem occurs when API is active and using the RC API clock as |
Add in a software delay so that STOP mode is re-entered at least 120us |
TIM_16B8C: Output compare pulse is inaccurate | MUCts04157 |
The pulse width of an output compare (which resets the free running |
The specification has been updated. Please refer to revision V02.07 (04 |
CPMU: High probabilty of PLL Loss of LOCK and UPOSC status change when using Adaptive Oscillator Filter with OSCBW=0 and high VCOCLK frequency | MUCts04170 |
A PLL configuration using the Adaptive Oscillator Filter with narrow |
The issue can be avoided by using wide bandwidth setting (OSCBW = 1 in |
PWM: Wrong output value after restart from stop or wait mode | MUCts04202 |
In low power modes (stop/p-stop/wait – PSWAI=1) and during PWM PP7 |
User software can be used to force the port PTP to the same level as |
PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | MUCts04205 |
When the PWM is used in 16-bit (concatenation) channel and the emergency |
If emergency shutdown mode is required: |
SCI: RXEDGIF occurs more times than expected in IR mode | MUCts04243 |
Configured for Infrared Receive mode, the SCI may incorrectly set the |
Case 1 and case 2 may occurs at same time. To avoid those unexpected |