NXP® Semiconductors | MSE9S12G240_0N95B |
Mask Set Errata | Rev. October 15, 2014 |
MC9S12G240, Mask 0N95B |
This errata sheet applies to the following devices: MC9S12G240, MC9S12G192 |
The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code. |
Device markings indicate the week of manufacture and the mask set used. The date is coded as four
numerical digits where the first two digits indicate the year and the last two digits indicate the work week.
For instance, the date code "0201" indicates the first week of the year 2002. |
Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix. |
MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum. |
Errata Number | Module affected | Brief Description | Work- around |
MUCts04243 | sci | SCI: RXEDGIF occurs more times than expected in IR mode | YES |
MUCts04258 | sci | SCI: RXEDGIF interrupt miss while enter STOP | YES |
SCI: RXEDGIF occurs more times than expected in IR mode | MUCts04243 |
Configured for Infrared Receive mode, the SCI may incorrectly set the |
Case 1 and case 2 may occurs at same time. To avoid those unexpected |
SCI: RXEDGIF interrupt miss while enter STOP | MUCts04258 |
If an active edge (falling if RXPOL=0, rising if RXPOL=1) on the RXD |
(1) If more than one edge with a minimum distance of 4 bus cycles occur, |