NXP® Semiconductors | MSE9S12DG64_4L86D |
Mask Set Errata | Rev. February 13, 2011 |
MC9S12DG64, Mask 4L86D |
This errata sheet applies to the following devices: MC9S12DG64, MC9S12DJ64, MC9S12D64, MC9S12A64, MC9S12D32, MC9S12A32 |
The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code. |
Device markings indicate the week of manufacture and the mask set used. The date is coded as four
numerical digits where the first two digits indicate the year and the last two digits indicate the work week.
For instance, the date code "0201" indicates the first week of the year 2002. |
Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix. |
MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum. |
Errata Number | Module affected | Brief Description | Work- around |
MUCts00628 | util | Key wake-up: Glitch filter exceeds upper 10us limit | YES |
MUCts00636 | util | MSCAN: Glitch filter exceeds spec limits | NO |
MUCts00681 | S12_bdm | Spurious SYNC pulse | YES |
MUCts00708 | spi | SPTEF flag set erroneously | YES |
MUCts00738 | atd_10b8c | flags in ATDSTAT0 do not clear by writing '1', ETORF erroneously set | YES |
MUCts00742 | spi | SPI in Mode Fault state, but MISO output buffer not disabled. | NO |
MUCts00789 | atd_10b8c | Write to ATDCTL5 may not clear SCF, CCF and ASCIF flags | YES |
MUCts00799 | spi | MISO not kept after sixteenth SCK edge. | YES |
MUCts00818 | crg | PLL: If osc_clock is 2 to 3 times pll_clock, STOP can cause SCM or reset | YES |
MUCts00828 | eets1k | STOP instruction may set EEPROM ACCERR flag. | YES |
MUCts00863 | fts64k | Flash: ACCERR is not set for a Byte Access | YES |
MUCts00876 | eets1k | EE: ACCERR is not generated for a Byte Access (MOVB instruction) | YES |
MUCts00902 | fts64k | STOP instruction while NVM CCIF=1 | YES |
MUCts01011 | ect_16b8c | ECT: Input pulse shorter than delay counter period recognised as a valid | YES |
MUCts01037 | atd_10b8c | CCF flags in ATDSTAT1 register might fail to set | NO |
MUCts01047 | eets1k | Write protection ineffective due to protection mirroring issue. | YES |
MUCts01053 | spi | SPIDR can be written without reading SPTEF flag as set | YES |
MUCts01103 | mscan | MSCAN: Time stamp corrupted in receive buffer | YES |
MUCts01965 | S12_bdm | Possible manipulation of return address when exiting BDM active mode | YES |
MUCts02415 | S12_mebi | MEBI: Missing ECLK edge on first external access after mode switching | YES |
MUCts03012 | eets1k | EEPROM Program Failure during Sector-Modify | YES |
MUCts03474 | atd_10b8c | ATD: Abort of an A/D conversion sequence with write to ATDxCTL0/1/2/3 may not work | YES |
MUCts03573 | mscan | MSCAN: Corrupt ID may be sent in early-SOF condition | YES |
MUCts03682 | atd_10b8c | ADC: conversion does not start with 2 consecutive writes to ATDCTL5 | YES |
MUCts04073 | pwm_8b8c | PWM: Emergency shutdown input can be overruled | YES |
MUCts04108 | ect_16b8c | ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1 | YES |
MUCts04151 | ect_16b8c | ECT_16B8C: Output compare pulse is inaccurate | YES |
MUCts04199 | pwm_8b8c | PWM: Wrong output value after restart from stop or wait mode | YES |
MUCts04203 | pwm_8b8c | PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode | YES |
Key wake-up: Glitch filter exceeds upper 10us limit | MUCts00628 |
The specified maximum pulse width limit of the key wake-up glitch filter |
The glitch filter now operates at a maximum pulse width limit of 14us. |
MSCAN: Glitch filter exceeds spec limits | MUCts00636 |
The specified MSCAN wake-up glitch filter pulse limits can be exceeded. |
None. |
Spurious SYNC pulse | MUCts00681 |
A spurious BDM SYNC pulse could be transmitted if the delay between |
Keep the delay between commands greater than 128 cycles. |
SPTEF flag set erroneously | MUCts00708 |
When the SPI is enabled in master mode, with CPHA bit set, back to back |
After the SPTEF flag has been set, a delay of 1/2 SCK period has to be |
flags in ATDSTAT0 do not clear by writing '1', ETORF erroneously set | MUCts00738 |
For the flags SCF, ETORF and FIFOR in ATDSTAT0 it is specified that |
SCF |
SPI in Mode Fault state, but MISO output buffer not disabled. | MUCts00742 |
When the SPI is in Mode Fault state (MODF flag set), according to the |
None. |
Write to ATDCTL5 may not clear SCF, CCF and ASCIF flags | MUCts00789 |
If a write to ATDCTL5 happens at exactly the bus cycle when an ongoing |
to abort a ongoing conversion use the recommended |
MISO not kept after sixteenth SCK edge. | MUCts00799 |
In SPI slave mode with CPHA set, MISO can change erroneously after a |
There are two possible workarounds for this problem: |
PLL: If osc_clock is 2 to 3 times pll_clock, STOP can cause SCM or reset | MUCts00818 |
This Erratum applies only to systems where PLL is used to divide down |
1) Avoid osc_clock/pll_clock ratios between 2 and 3. |
STOP instruction may set EEPROM ACCERR flag. | MUCts00828 |
If the ECLKDIV EEPROM clock divider register has been loaded, and the |
The ACCERR bit in the ESTAT register must be cleared after the execution |
Flash: ACCERR is not set for a Byte Access | MUCts00863 |
Starting a command sequence with a MOVB array write instruction (Byte |
Avoid the use of MOVB instruction for array program operations. |
EE: ACCERR is not generated for a Byte Access (MOVB instruction) | MUCts00876 |
Starting a command sequence with a MOVB array write instruction (Byte |
Avoid the use of MOVB instruction for array program operations. |
STOP instruction while NVM CCIF=1 | MUCts00902 |
If the FCLKDIV flash clock divider register has been loaded, and the |
The ACCERR bit in the FSTAT register must be cleared after the execution |
ECT: Input pulse shorter than delay counter period recognised as a valid | MUCts01011 |
According to the observation, input pulse (high/low) whose pulse width |
A software workaround is available. |
CCF flags in ATDSTAT1 register might fail to set | MUCts01037 |
The setting of the CCF7-0 flags in ATDSTAT1 register |
None. |
Write protection ineffective due to protection mirroring issue. | MUCts01047 |
The 1Kb EEPROM module can be mapped to any 2Kb boundary and is mirrored |
Ensure the EEPROM is only accessed in the upper 1Kb of the 2Kb area |
SPIDR can be written without reading SPTEF flag as set | MUCts01053 |
On the first instance after MCU reset, the SPIDR data register can be |
Do not attempt to write the SPIDR data register without first checking |
MSCAN: Time stamp corrupted in receive buffer | MUCts01103 |
When the foreground receive buffer (RxFG) is read, with the Receiver |
The application software has to ensure to read the receive messages in |
Possible manipulation of return address when exiting BDM active mode | MUCts01965 |
Upon leaving BDM active mode, the CPU return address is stored |
Avoid using the BGND instruction when the ENBDM bit in the BDMSTS |
MEBI: Missing ECLK edge on first external access after mode switching | MUCts02415 |
If the ECLK is used as an external bus control signal (ESTR=1) the first |
Enter expanded mode with ECLK output disabled (NECLK=1). Enable the ECLK |
EEPROM Program Failure during Sector-Modify | MUCts03012 |
At oscillator frequencies above 4MHz the Program step of the EEPROM |
Use seperate Erase and Program commands in place of the Sector-Modify |
ATD: Abort of an A/D conversion sequence with write to ATDxCTL0/1/2/3 may not work | MUCts03474 |
Starting a conversion with a write to ATDxCTL5 or on an external |
Only write to ATDxCTL4 to abort an ongoing conversion sequence. |
MSCAN: Corrupt ID may be sent in early-SOF condition | MUCts03573 |
The initial eight ID bits will be corrupted if a message is set up for |
Due to increased oscillator tolerance a transmission start in the third |
ADC: conversion does not start with 2 consecutive writes to ATDCTL5 | MUCts03682 |
When the ATD is started with write to ATDCTL5 |
Only write once to ATDCTL5 when starting a conversion. |