| Channel 0 – 3 Input Capture interrupts are inhibited when BUFEN=1,
LATQ=0 and NOVWx=1 if an Input Capture edge occurs during or between a
read of TCx and TCxH or between a read of TCx/TCxH and clearing of CxF.
Details:
When any of the buffered input capture channels 0 - 3 are configured
for buffered/queue mode (BUFEN=1, LATQ=0) each of the channel’s input
capture holding registers and each channel’s associated pulse
accumulator and its holding register are enabled. When the input
capture channel is enabled by writing to a channel’s EDGxB and EDGxA
bits, both the input capture and input capture holding register are
considered empty. The first valid edge received after enabling a
channel will latch the ECT’s free running counter into the input
capture register (TCx) without setting the channel’s associated CxF
interrupt flag. The second valid edge received will transfer the value
of the input capture register, TCx, into the channel’s TCxH holding
register, latch the current value of the free running timer into the
input capture register and set the channel’s associated CxF interrupt
flag. In this condition, both the TCx and TCxH registers are
considered ‘full’.
If a corresponding channel’s NOVWx bit in the ICOVW register is set,
the capture register or its holding register cannot be written by a
valid edge at the input pin unless they are first emptied by reading
the TCx and TCxH registers. The act of reading the TCx and TCxH
registers and clearing the channel’s associated CxF interrupt flag
involves three separate operations. Two 16-bit read operations and an 8-
bit write operation.
If a channel’s associated CxF interrupt flag is cleared before reading
the TCx and TCxH registers and if a valid input edge occurs during or
between the reading of the capture and holding register, a channel’s
associated CxF interrupt flag will no longer be set as the result of
valid input edges. For example:
Clear CxF
|
|
V
Read TCx <----+
| |
|<--------+--- Valid Input Edge Occurs
V |
Read TCxH <---+
If the TCx and TCxH registers are read before a channel’s associated
CxF interrupt flag is cleared and if a valid input edge occurs between
the reading of TCx/TCxH and the clearing of a channel’s associated CxF
interrupt flag, a channel’s associated CxF interrupt flag will no
longer be set as the result of valid input edges. For example:
Clear CxF
|
|
V
Read TCx
|
|<------------ Valid Input Edge Occurs
V
Read TCxH
Systems that service the interrupt request and read the TCx and TCxH
registers before the next valid edge occurs at a channel’s associated
input pin will avoid the conditions under which the errata will occur.
|