In the first part of our blog series we focused
myth busting contactless payments. Now we move to the other side of the payment transaction – the
Point-Of-Sale (POS)
infrastructure point of view where there is growing demand for machines
enabled to process contactless payments. In fact, over 50% of the POS
terminals are already contactless-enabled and only need to activate the
function when the merchant is ready (ABI, 2013). The market for
NFC
enabled
POS
terminals is expanding quickly, and is expected to maintain rapid growth
through 2019 (Berg Insight, 2015). Payment network operators Mastercard and
Visa are pushing NFC
acceptance until the end of the decade for all payment terminals. And that
means people with
NFC-enabled cards and smartphones will have more places to make contactless
payments.
Mobile point-of-sale (mPOS) terminals
Also in the mix is the mobile POS
(mPOS) sector, a new distinct category of payment terminals experiencing
exponential growth. Of particular note is the fact that small and micro
businesses, which traditionally are cash-only, are adopting mPOS
formats to support contactless payments by card or NFC-enabled smartphone. For example,
in the past few years, consumers have
purchased fares from many independent taxis, meals from the growing gourmet
food trucks, knick-knacks at trade fairs or even products at a
farmer’s market with their cards using an mPOS
terminal. These devices are cost-efficient, portable, secure, fast to install and they’re catching on quickly. Roughly 50 million are expected to be
in use by 2018.
Laptops and tablets as payment terminals
For online retailers, there’s always been a certain amount of risk
associated with accepting credit card payments, because the cardholder
can’t physically present the card to complete the transaction. With
“tap-to-pay,” your laptop or tablet is equipped with a secure
reader module so that you can tap your payment card or NFC
enabled smartphone to the device and confirm its presence. With “in-app
payment,” your mobile device is equipped with a secure element IC that
stores your credentials in a trusted, verified format. Either way, you get an
easier method for using your card, as you don’t have to type in any
numbers to complete a transaction, and retailers and banks can be more certain
that you are the actual owner of the card.
Embedded modules for payment from any device
The
technologies that enable secure mobile payments can be implemented in an
embedded module that can then be integrated into just about any device.
Imagine a future when payment functionality finds its way into a new
generation of applications. Purchase inkjet cartridges from your printer, buy
groceries from your refrigerator, pay for a hotel reservation from your
car’s dashboard – embedded modules will make it all possible.