NXP’s new Touch solution accelerates time to market with pre-certified and tested hardware components, optimized software environment and easy-to-use configuration toolsSAN JOSE, Calif., June 20, 2017 (GLOBE NEWSWIRE) -- NXP Semiconductors N.V. (NASDAQ:NXPI) is launching and showcasing its new NXP Touch solution today at the NXP FTF Tech Forum. This solution combines specialized touch software with the Touch Sense Interface (TSI) module available on the Kinetis KE15Z MCU along with a complete set of tools enabling designers to easily add touch to user interface designs on IoT applications including home appliances, smart buildings, machines for industrial control and more.
Adding touch to a user interface can be a challenging task as there are many factors involved to ensure a successful user experience. The NXP Touch solution addresses these challenges and reduces the complexity involved with implementing touch thereby speeding time to market. Key aspects of the NXP Touch solution include:
- Two operation modes (self-cap and mutual cap)
- Advanced robustness in electromagnetic compatibility (EMC)
- Pre-certified and tested hardware, including IEC61000-4-6 certification for 3V and 10V
- Water and other liquid resilience (waterproof)
- High sensitivity and resolution
- Optimized software, including NXP Touch Library and SDK touch APIs support
“The large developer presence at the FTF Tech Forum provides an ideal platform to launch the new Touch solution, which reaffirms our commitment to helping the developer community quickly and easily innovate new mass market and IoT applications,” said Geoff Lees, senior vice president and general manager of the microcontroller business. “The NXP Touch solution now integrates high-level APIs and offers GUI tools to support the development demands of our customers.”
The benefits of Kinetis KE15Z MCUs’ easy-to-integrate hardware includes pre-certification for (EMC, liquid toleration and noise immunity to prevent long design cycle times. The robust Kinetis KE15Z MCU is compliant with IEC61000-4-2, -4-4, 4-6 and IEC60730 class B standards to protect product and consumers in end designs by ensuring the voltage and temperature of the device remains within safe parameters. Additionally, the NXP Touch solution enables developers to create code easily with the integration of auto tuning and parameter configurations that include touch sensitivity, touch response time and power consumption, for example.
NXP Touch Software is optimized for the Kinetis KE15Z MCUs and its Touch Sense interface hardware module integrated. The software is integrated into the MCUXpresso development environment for ease of development. The solution is also supported by the FRDM-KE15Z hardware development platform.
Pricing and Availability
NXP Touch software, FRDM-KE15z and FRDM-TOUCH development boards are available beginning today, June 20, 2017. For pricing or additional information, please contact a local NXP sales office.
For more information regarding NXP’s new TSI, please visit: www.nxp.com/Touch.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security and privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 31,000 employees in more than 33 countries and posted revenue of $9.5 billion in 2016. Find out more at www.nxp.com.
NXP, the NXP logo, and Kinetis are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2017 NXP B.V.
For more information, please contact:
![Primary Logo](https://resource.globenewswire.com/Resource/Download/15138703-6ac6-4e52-9366-3215f59f8599?size=1)
NXP Semiconductors Netherlands B.V.