Sign in for a personalized NXP experience.
NXP cybersecurity engineering processes are now certified as compliant with the new automotive cybersecurity standard ISO/SAE 21434.
Compliance with ISO/SAE 21434 aligns with the existing NXP principle of security-by-design in automotive applications.
NXP is the first semiconductor supplier to be certified by TÜV SÜD to comply with the latest automotive cybersecurity standard ISO/SAE 21434. The new automotive cybersecurity standard aims to provide connected vehicles with robust protection from malicious cyberattacks. The standard requires OEMs and their supply chains to apply a security-by-design approach to their components, servers, and processes to reduce the risk of being vulnerable to attacks at any point in the vehicle lifetime, from the initial concept and design phases to end of life.
From July 2022 onward, vehicle manufacturers (automotive OEMs) must comply with the R155 automotive cybersecurity regulation for new vehicle type launches in Europe, Japan and Korea, which represents over a third of global vehicle production. Other regions are expected to follow. The standard ISO/SAE 21434 supports the implementation of the R155 requirements in organizations across the supply chain. The NXP ISO/SAE 21434 certification helps enable OEMs to meet requirements of the R155 regulation.
Connected vehicles will inevitably communicate with outside entities, from other vehicles, to smart city infrastructure and to the cloud. If left unsecured, the vehicle electronics systems could be compromised by attackers. Robust security measures are essential to prevent attacks and protect the vehicle, its systems and the back-end networks that serve them from cyberattacks.
NXP leverages its long-standing expertise in security to address the needs of the auto industry. The existing policies and processes of NXP have been refined and extended to fully meet the requirements of the new standard ISO/SAE 21434.
The assessment and certification was conducted by TÜV SÜD, a trusted partner of choice for safety, security and sustainability solutions. TÜV SÜD audited NXP’s organization, its policies and processes for compliance with new standard ISO/SAE 21434.
“With the increasing number of connected vehicles and technologies, it puts security at the forefront. The certification facilitates the security by design approach, enhancing trustworthiness and reducing complexity across the complex automotive supply chain.”
Claudio Gregorio, Department Manager Functional Safety and Cybersecurity at TÜV SÜD
For more information, visit nxp.com/security.
NXP Semiconductors N.V. (NASDAQ: NXPI) enables secure connections for a smarter world, advancing solutions that make lives easier, better, and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the automotive, industrial & IoT, mobile, and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 29,000 employees in more than 30 countries and posted revenue of $8.61 billion in 2020. Find out more at www.nxp.com.
NXP, the NXP logo and EdgeLock are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2021 NXP B.V.