Sign in for a personalized NXP experience.
LAS VEGAS, Jan. 04, 2022 – NXP® Semiconductors (NASDAQ: NXPI) today announced the IW612, the industry’s first secure tri-radio device to support the Wi-Fi 6, Bluetooth 5.2 and 802.15.4 protocols. Part of NXP’s new family of tri-radio products, the new device enables seamless, secure connectivity for smart home, automotive and industrial use cases, and supports the new groundbreaking Matter connectivity protocol. The IW612 frees consumers from the restrictions of single protocol ecosystems, allowing them to enjoy seamless interoperability across different ecosystems and wireless network technologies. Additionally, developers benefit from NXP’s state-of-the-art coexistence capability, which enables simultaneous support of three radios on a single device, reducing costs and development time.
One of the primary challenges facing the IoT is limited interoperability, which can restrict the consumer’s ability to mix smart home products from different companies. Matter, a new standardized IoT connectivity protocol, designed by a consortium of industry leaders including NXP, addresses these limitations by unifying how devices communicate, independent of the manufacturer or wireless technology. The protocol creates more connections between more objects, thereby simplifying development for manufacturers and compatibility for consumers.
To support a new era of interoperability, the IW612 integrates three of the industry’s leading connectivity radios onto a single device for the first time, delivering robust radio performance and integrating a high-performance RF front end. This technology combination enables true interoperability in the smart home, significantly reducing development time, simplifying design and reducing costs. The highly integrated solution overcomes hardware co-existence challenges that developers face today, while also enabling advanced security protocols to help thwart the ever-increasing number of security threats faced by the IoT.
The IW612 leverages NXP’s long history of leadership in providing secure solutions to help combat the ongoing security threats smart devices face. The IW612 offers secure boot, debug and over-the-air firmware updates for ongoing protection, as well as WPA3 security and hardware encryption engines.
"With the IW612, developers can leverage different wireless connectivity protocols on a single device to create an easy-to-use, secure product for smart home, industrial and automotive use cases. From door locks and smart speakers to in-vehicle entertainment and telematics, products can now benefit from our tri-radio solutions that address multiple technologies and ecosystems, including Matter. This provides developers with a more cost-effective solution while streamlining deployment for the consumer."
- Larry Olivas, Vice President and General Manager for Wireless Connectivity Solutions, NXP Semiconductors.
"Interoperability has been a key challenge that has fragmented the smart home market for years, but Matter-enabled devices can change that. With its new monolithic devices, NXP enables developers to leverage Matter-supported connectivity protocols for their smart home applications and help accelerate Matter adoption. This, in turn, will provide consumers with improved useability by making smart devices easier to connect and greater choice among the interoperable devices they can use."
- Jonathan Collins, Research Director at ABI Research.
The IW612 is an ideal solution for border routers, bridges and gateways in the smart home that require connecting Thread or Bluetooth devices to the cloud using the integrated Wi-Fi 6 radio. Additionally, the IW612 enables communication between Matter devices regardless of whether the devices use Wi-Fi or Thread. This allows Matter-over-Wi-Fi products to control and monitor Matter-over-Thread devices, and vice versa, for seamless interoperability.
Key features of IW612 include:
The IW612 is sampling now and will be demonstrated live at CES 2022. For more information, please visit NXP.com/Matter or contact NXP Sales worldwide.
With one of the industry’s broadest portfolios of wireless technologies, NXP is committed to accelerating our vision of a connected world that anticipates and automates. When combined with the processing power of the EdgeVerse platform, NXP is uniquely positioned to enable smart connected devices – making lives easier, safer, and more convenient. Whether it’s connecting people to the Internet, joining IoT devices to the cloud, or communicating with cars in new and unexpected ways, NXP’s portfolio allows customers to advance their most innovative ideas with confidence and a sense of trust. By collaborating with our partners, we are connecting our world and delivering solutions that advance society together.
NXP Semiconductors N.V. (NASDAQ: NXPI) enables secure connections for a smarter world, advancing solutions that make lives easier, better, and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the automotive, industrial and IoT, mobile, and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 29,000 employees in more than 30 countries and posted revenue of $8.61 billion in 2020. Find out more at www.nxp.com.
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2021 NXP B.V.
View this press release in German
Tags: Corporate, Industrial
Photo:NXP Advances IoT Connectivity with Industry’s First Secure Tri-Radio Device Image.
Download photo (1MB).
View this press release in PDF