LONG BEACH, Calif.,
The RFE Series features a multi-level portfolio that addresses each step for building a successful
With the lab box, system developers will be able to create prototypes quickly and cost effectively. Once the proof of concept is complete, engineers can leverage the module and pallet to accelerate the design of their production system. In addition, NXP is building an ecosystem of skilled and vetted design houses and ODM partners to receive customized, production-ready solutions faster.
“Our RFE Series features tools to speed up the development of RF systems,” said Pierre Piel, senior director and general manager for multi-market RF power at NXP. “Like Matryoshka dolls, we are wrapping up NXP’s RF transistors with multiple levels of hardware and software that minimizes the complexity involved in developing RF Energy systems.”
Unlocking Innovation
Transistors are bringing RF power systems using vacuum tubes to the next level.
Key features:
“Solid-state RF energy is set to revolutionize various markets ranging from consumer cooking to medical ablation to industrial heating and more, where precision, flexibility and repeatability is crucial,” said Dr. Klaus Werner, executive director of the
Pricing and Availability
NXP debuts its RFE Series at 2.45 GHz, 250 W, with full availability in
Note: These prices are suggested resale prices through NXP approved suppliers.
All three solutions are built around NXP’s flagship MRF24300N 300 W LDMOS transistor, designed for 2400-2500 MHz operations at 60 percent drain efficiency. The MRF24300N RF transistor is shipping in volume and is part of NXP’s Product Longevity Program guaranteeing availability until at least 2026.
To learn more, visit NXP at IMPI or at www.nxp.com/RFenergy.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 30,000 employees in more than 30 countries and posted revenue of $9.26 billion in 2017. Find out more at www.nxp.com.
For more information, please contact:
Americas | Greater China/Asia | Europe | |||
Jacey Zuniga | Esther Chang | Martijn van der Linden | |||
Tel: +1 512-895-7398 | Tel: +886 2 8170 9990 | Phone: +31 6 1091 4896 | |||
Email: jacey.zuniga@nxp.com | Email: esther.chan@nxp.com | Email: martijn.van.der.linden@nxp.com |
Photos accompanying this announcement are available at
http://www.globenewswire.com/NewsRoom/AttachmentNg/ea7a57f3-2f56-46e0-b1e8-0e15b07be7a6
http://www.globenewswire.com/NewsRoom/AttachmentNg/fff3283c-b55b-4cfb-a4d3-45f3df54a37a
Tags: Industrial