Increased functionality, stronger security and advancements to consolidated mobile IDs are changing the future of travel
Out of 900 million passports issued, 730 are ePassports, which now represent the majority of passports in circulation. According to the
Trend #1: Increasing Functionality
ePassport functionality is continuously evolving. ICAO first introduced BAC (Basic Access Control), then EAC (Extended Access Control) and today is currently migrating to SAC (Supplemental Access Control) protocols. All ePassports use the same data format, known as the Local Data Structure (LDS), to store and “seal” data to protect it from tampering. The data that is embedded in the chip remains the same for the whole lifespan of the document and can’t be modified. A new format called LDS2, which is a backwards-compatible extension to previous generations of electronic passports and not far away from publication, will change that. It enables the digital storage of travel data such as electronic visas and travel stamps directly on the chip, and allows the complete passport booklet to be available in digital format. In addition, the read-and-write capacity allows new biometric data to be added. Countries will have more choice in national policy, and give people the option of submitting biometrics if they want to participate in a trusted-traveller program. Introducing the concept of passport applications opens up opportunities to efficiently automate the processing of passengers and their documents. This frees up time at borders so officials can attend to more high-value activities, and increase return on investment in the border-clearance infrastructure.
NXP’s long-standing expertise in supporting ePassport solutions around the world has led to a huge existing infrastructure enabling easier integration of international traveller programs. Currently, NXP ships SAC solutions globally in high volume, and NXP is fully involved in the definition and standardization of ePassport LDS2 and has developed a solution that successfully passed initial ICAO compliance tests performed by the ICAO NTWG.
Trend #2: Stronger Security
The European refugee crisis, the rise in international terrorism and the increase in criminal activity spiked the demand for stolen and forged passports. This development advances the distribution of ePassports on a global scale. Countries that already issue ePassports are looking to increase the security further. As a result, the future will see more data being transferred from the physical pages of an ePassport, to the secure and tamper-resistant Integrated Circuit (IC). The IC is designed to resist attempts to steal, modify or misuse the data, and ceases to work properly if physically tampered with.
In reality, the chip in the electronic passport has more capacity and functional flexibility than just supporting the ICAO 9303 protocols, which offers untapped opportunities to implement electronic forensic security features. It provides functionality that may be used on an international and/or national level, depending on feature implementation and international cooperation. Customer-specific functionality implemented in the chip can introduce additional security and efficiency in the process of border management and can elevate document security and fraud prevention to an unprecedented level.
NXP’s SmartMX secure microcontroller family with its world-class security features make up the core component for secure identity programs. SmartMX products contain the IntegralSecurity architecture with more than 100 security mechanisms representing a true benchmark in security and are currently ready to support custom-specific electronic forensic features.
Trend #3: ePassport Complemented by “Virtual Mobile Identity”
Answering the demand for leaner administration and stronger security, the ePassport is evolving from “just” being a travel document to being a government-issued root credential for other applications, including a “virtual mobile identity.” In the future, the single, secure digital ID in combination with technology such as NFC, will allow ePassport owners to identify themselves, to interact with and authenticate applications via NFC-enabled mobile smartphones or wearable formats. ICAO is using the 9303 NTWG (
NXP is an NFC co-inventor, and its SmartMX product family is the preferred choice for the secure element of NFC-enabled smartphones. NXP is also involved in ISO and ICAO standardization activities for “virtual mobile identities.” The combination of technology know-how and expertise in eGovernment solutions is a valid reason to trust NXP as a partner for mobile-based government solutions.
Future advancements in flexibility, accessibility, security and interoperability of the ePassport ecosystem will allow users to securely derive credentials to other electronic devices beyond passports, including mobile phones. For the secure chip in the document to serve these trends, ultra-thin design, larger memory as well as higher cryptography and communication speeds are required.
Image caption:
95 of the 120 ICAO member states issuing ePassports qualified NXP technology.
About
NXP, the NXP logo and SmartMX are trademarks of
For more information, please contact:Americas Tate Tran Tel: +1 408-802-0602Email: tate.tran@nxp.comEurope Martijn van der Linden Tel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China /AsiaEsther Chang Tel: +886 2 8170 9990Email: esther.chang@nxp.com
Tags: Industrial