BERLIN,
|
A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/d85efe70-c4ab-4e85-ad95-ae00b3de308a
The secret to efficient and effective heating, delivered by the Midea appliance, is NXP’s MHT1004N, a low-voltage solid state cooking transistor which creates and delivers energy in an effective and efficient way. The component enables greater control over the heating process and allows the Midea appliance to control energy in a closed loop manner for evenly heated food. The semiconductor cooking method also enables consistent results thereby enabling smart features for internet-connected appliances.
“We’re excited to team up with NXP and transform the conventional methods of cooking to solid state,” said Luan Chun, director of the appliances business unit innovation center at Midea. “Together, we’ve also jointly developed a standard system unit, which enables us to quickly implement new designs using a flexible, modular approach for future product developments.”
"Midea and NXP have been cooperating for years to research and develop solutions for the future smart kitchen,” said Mr. Wu Dong, senior director of RF products at NXP Semiconductors Asia Pacific. “This new appliance calls upon our years of collaborating and innovating together with the same vision -- to usher in a smarter cooking experience into consumers’ kitchens.”
The new product from Midea is based on the MHT1004N, the latest generation cooking component from NXP. The MHT1004N is specifically developed as a 300 watt cooking device. For more information about NXP RF cooking technology, visit www.nxp.com/RFcooking.
Demonstration
The new kitchen appliance will be demonstrated at IFA 2016 in Berlin, Germany in Midea’s booth, Hall 7.1a/101
About NXP
NXP and the NXP logo are trademarks of
For more information, please contact:AmericasTate TranTel: +1 408-802-0602Email: tate.tran@nxp.comEuropeMartijn van der LindenTel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China / AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chang@nxp.com
Tags: Industrial