The JN516x ZigBee 3.0 SDK must beinstalled on top of the BeyondStudio for NXP toolchain (JN-SW-4141).Installation instructions are provided in the BeyondStudio for NXP Installationand User Guide (JN-UG-3098). Application Notes are also available that provideZigBee 3.0 demonstration applications that can be run on the components of the JN516x-E004 Evaluation Kit and used as a starting point forcustom application development. EK004 also supports NFC commissioning, as withNXP's earlier ZigBee solutions.
ZigBee 3.0 helps facilitate a simpleend-user experience with set-up and operation.
Availability
ZigBee-3.0 beta SDK registration isavailable now. For more information, click here.
Tags: Industrial