NXP releases i.MX 8XLite SoC to address secure V2X and industrial IoT applications.
NXP Semiconductors has announced the release of its new i.MX 8XLite applications processor focused on secure V2X and industrial IoT applications. The SoC features NXP’s integrated EdgeLock® security and is targeted to meet FIPS 140-3 while simultaneously executing highly complex cryptography and processing telematics data. FIPS 140-3 is a U.S. government security standard for cryptographic modules used in a variety of applications, including V2X and critical infrastructure applications.
The advanced applications processor offers carmakers the opportunity to expand V2X benefits to entry level vehicles. It enables fleet management for automated vehicles and reduces operational costs via enhanced traffic control, improved traffic flow and optimized path planning. Industrial IoT developers can leverage the SoC in secure wireless, Ethernet and control area networking (CAN) applications such as industrial vehicle management, building control and safety systems, solar power generation, EV charging stations, access controllers and more.
The i.MX 8XLite SoC is a member of the i.MX 8 series of applications processors, purpose-built with a V2X accelerator, which can be leveraged as part of NXP’s RoadLink® V2X solution or as a standalone accelerator. Its vehicle-to-infrastructure capability helps vehicles communicate with roads, bridges and roadside units to obtain information about road conditions ahead. Its car-to-car communication enables cars to communicate via wireless technologies such as IEEE® 802.11p, 5G and cellular, creating a network of similarly equipped vehicles to “see” further ahead.
“We believe road safety is for everyone, and it should scale across vehicles and devices,”
"The i.MX 8XLite SoC offers the security and performance needed to expand the safety benefits of V2X into entry level vehicles and into exciting new realms of unmanned industrial delivery and drone applications.”
Dan Loop, General Manager, Automotive Edge Processing, NXP
For more information, visit nxp.com/iMX8XLite.
NXP Semiconductors N.V. (NASDAQ: NXPI) enables secure connections for a smarter world, advancing solutions that make lives easier, better, and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the automotive, industrial and IoT, mobile, and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 29,000 employees in more than 30 countries and posted revenue of $8.61 billion in 2020. Find out more at. www.nxp.com.
NXP, the NXP logo and EdgeLock are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2021 NXP B.V.
Tags: Corporate, Industrial and IoT