Only about 20% of U.S. consumers have used contactless payment systems such as Apple Pay, Samsung Pay and Android Pay to make retail purchases, according to the study, conducted by market research firm
“More than half of U.S. consumers have little or no familiarity with various forms of contactless payment technology. We feel this is largely because retailer implementation has been lackluster,” said Ben Bajarian, director of the consumer technology practice at Creative Strategies. “Lack of education remains the largest barrier to widespread adoption in the U.S.”
A majority of U.S. consumers reported they would use contactless payment for over half their purchases if they knew that form of payment was supported, with 45-59 year olds being the age range to most often use contactless for every single transaction. In contrast, 30-44 year olds in
“The new research from Creative Strategies demonstrates that consumers who use contactless payment systems are overwhelmingly satisfied with the convenience and speed of the experience. It’s doing away with the need to carry cash or a check book—just wave your smartphone or card in front of the payment terminal. Plus, it’s more secure,” said
The survey also found that 40% of US consumers would be likely or highly like to use contactless payment more often if they were offered exclusive loyalty points/perks or exclusive discounts. In all three markets, consumers said they were looking to the retailers to educate them on the security benefits of contactless payments.
Among U.S. consumers who do use contactless payment technology, 77% reported that they were satisfied or very satisfied with the experience.
NXP is publicizing the research produced by Creative Strategies as a way to encourage broader adoption of contactless payment technology in the U.S. As a broad supplier of semiconductor products, NXP offers solutions for contactless payment connectivity, including Near Field Communication (NFC), security, software and services.
Details for research findings will be presented at an event hosted by NXP during Money 2020 in
About NXP
NXP and the NXP logo are trademarks of
For more information, please contact:Americas Tate TranTel : +1 408-802-0602Email: tate.tran@nxp.comEurope Martijn van der Linden Tel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China /AsiaEsther Chang Tel: +886 2 8170 9990Email: esther.chang@nxp.com
Tags: Consumer, Industrial