New Module Makes it Easy to Incorporate NFC as a Smart Add-on for Almost any Electronic Device;
“The new plug-and-play NFC click board™ powered by NXP enables the full range of NFC application for Hexiwear devices. It provides the most streamlined and easy way to take advantage of NFC infrastructure already in place," said Dr.
The NFC click Module for Hexiwear removes the complexity of NFC integration by enabling developers to easily leverage the full potential of NFC in Card Emulation, Read/Write and Peer-to-Peer Modes with NXP’s PN7120 chip, which is ideal for designing prototypes intended to interact with existing NFC infrastructure or prototype new ideas. All necessary NFC drivers are included in the Hexiwear SDK.
NFC click is also compatible with other development platforms, including NXP’s Freedom development boards, which are small, low power, cost-effective evaluation and development platforms for quick application prototyping and demonstration of Kinetis MCU families.
“NXP believes in the market potential that our developer partners will bring with their innovative mindset and the new NFC click module is aimed at providing the tools necessary to quickly bring their ideas for smart NFC interactions to life,” said
NFC click and NXP PN7120 details
Developed by MikroElektronika, in partnership with NXP, NFC click has full compliancy with
NXP plans to release an additional NFC click add-on board based on NTAG I²C plus, NXP’s range of connected NFC tags, in Q1 2017.
Hexiwear information
Hexiwear is a complete open-source platform that combines the style and usability of high-end consumer devices with the functionality and expandability of sophisticated engineering development platforms, making it the ideal form factor for IoT edge node and wearable markets. At the core of Hexiwear is the low power, high-performance Kinetis K6x microcontroller, the Kinetis KW4x multimode radio System on Chip (SoC) supporting BLE, six sensors, external flash memory, a color OLED display and a rechargeable battery. Android and iOS support is straightforward with open source, customizable applications.
About MikroElektronika
MikroElektronika is a renowned producer of a wide range of hardware and software development tools for various microcontroller architectures, including compilers for three languages: mikroC, mikroBasic and mikroPascal. The company is also known as the originator of mikroBUS™ — a well-established standard for add-on boards compatible with their offering of hundreds of sensor and transceiver add-on boards called click boards™. MikroElektronika's goal is to provide software and hardware tools that are easy to use, save time and help get the job done quickly. This approach attracts both hobbyist and professionals. Learn more at www.mikroe.com.
About
NXP, the NXP logo and Kinetis are trademarks of
For more information, please contact:Americas Tate Tran Tel: +1 408 802 0602Email: tate.tran@nxp.comGreater China /AsiaEsther Chang Tel: +886 2 8170 9990Email: esther.chang@nxp.comEurope Martijn van der Linden Phone: +31 6 1091 4896Email: martijn.van.der.linden@nxp.com
Tags: Consumer, Industrial