Sign in for a personalized NXP experience.
SAN JOSE, Calif.,
|
NXP’s Loader Service solution simplifies the development and integration of payment functionality while maintaining significantly lower setup and maintenance costs. Users can simply add their card information to the Garmin Pay wallet, powered by
“NXP is recognized as the preferred provider in the payment ecosystem, known for our ability to deliver trusted security, authentication, and end-to-end NFC solutions into many of the world’s most high-profile applications,” said Rafael Sotomayor, senior vice president and general manager of secure transactions and identifications at NXP. “NXP’s PN80T SE and NFC solution enable Garmin and others to quickly bring to market secure and convenient payment experiences.”
Smart, sturdy and stylish, the vívoactive 3 smartwatch has built-in GPS and comes with over 15 preloaded sports apps. Featuring fitness and wellness monitoring tools like fitness age and all-day stress tracking, the vívoactive 3 is the perfect accessory for playing and paying. The new Forerunner 645 Music features integrated music, performance monitoring tools and advanced running dynamics to help athletes get the data they need. Whether out for a run with friends, gearing up for race day or stopping for a quick bite to eat, the Forerunner 645 Music is easy to wear all day, every day. Garmin major Pay supports Mastercard and Visa debit and credit cards from an increasingly expanding portfolio of issuing banks. Having these cards in their Garmin Pay wallet gives users the same rewards and benefits of the physical cards, with the convenience of having them right on the wrist.
“In collaborating with NXP, we can better provide the ultimate on-the-go lifestyle to our customers,” said Dan Bartel, Garmin vice president of worldwide sales. “This technology, featured on the vívoactive 3 and Forerunner 645 Music, enables customers to leave their cash and credit cards at home and securely make purchases where NFC payments are accepted.”
“We want to give our cardholders the choice and peace of mind to make more secure digital payments from a variety of connected devices through a tap or touch,” said Kiki Del Valle, senior vice president, Commerce for Every Device, Mastercard. “By integrating Mastercard token services with the NXP platform, we will create EMV-like security for every transaction and bring in the simple, speedy and secure payment experience that consumers have come to expect from Mastercard.”
About the PN80T NFC Solution
Leveraging its many large volume deployments for mobile phone applications, NXP is now leading the way in delivering mobile payment technology for wearables. The company’s PN80T solution is the industry’s first 40nm SE and uniquely addresses the critical industry challenges of size, power consumption, security, performance, and ease-of-integration for the growing wearable device market. The innovative chip solution combines best-in-class RF performance, exceptional flexibility in NFC antenna design and state-of-the-art Secure element performance, which results in fast transaction times and field updates – consequently leading to better end-user experiences. Included in the PN80T and the company’s PNXX family of NFC modules, NXP’s Loader Service comes preconfigured on the module’s secure element so that developers have immediate access to the Loader Service. This provisioning solution allows any service provider, small or large, local or global, to easily deploy secure NFC applications.
For more information visit: https://www.nxp.com/products/identification-and-security/nfc:MC_71110.
– End –
About NXP Semiconductors
NXP and the NXP logo are trademarks of
About
The ever-expanding Garmin fitness segment develops technologies to enhance and promote healthy and active lifestyles. Whether users are runners, cyclists, swimmers, multi-sport athletes, or simply looking to stay active throughout the day, there is a Garmin product that can help them reach their health and fitness goals. For decades, Garmin has pioneered new GPS navigation and wireless devices and applications that are designed for people who live an active lifestyle. Garmin serves five primary business units, including automotive, aviation, fitness, marine, and outdoor recreation. For more information, visit Garmin's virtual pressroom at garmin.com/newsroom, contact the Media Relations department at 913-397-8200, or follow us at facebook.com/garmin, twitter.com/garmin, or youtube.com/garmin.
For more information, please contact: | ||
Americas | Europe | Greater China / Asia |
Tate Tran | Martijn van der Linden | Esther Chang |
Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +886 2 8170 9990 |
Email:tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: esther.chang@nxp.com |
A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/70347b71-cbdb-4b21-9c19-de79836c8926
Tags: Consumer, Industrial