First of Four New NFC Solutions Released to Quicken Design Process and Ensure Robust Operation in Challenging EnvironmentsEINDHOVEN, Netherlands, Dec. 28, 2015 (GLOBE NEWSWIRE) -- With the flagship solution, PN5180, NXP Semiconductors N.V. (NASDAQ:NXPI), co-inventor of Near Field Communication (NFC), today announced the beginning of a new era in the evolution of NFC to bring intuitive proximity technology everywhere. PN5180 is an advanced, multi-protocol (ISO/IEC 15693, Felica™, MIFARE® and ISO/IEC 14443A/B) NFC frontend that delivers more efficient, robust, and reliable operation, even in harsh environments. Building on the success of the PN512, PN5180 delivers four times more output power and is designed to enable state-of-the-art readers for contactless payment without the need of an additional booster.
“NFC moves increasingly into new and more demanding applications, now transportation terminals need to support EMV payment schemes and have to interact with new payment or transit form factors like NFC-enabled phones, wearables and even rings. The requirements for performance, reliability and interoperability therefore expand,” said Pradip Mistry, vice president of research and development at Cubic Transportation Systems. “NXP succeeds to bring NFC to the next level in technology with the PN5180 and its new features like Dynamic Power Control and Adaptive Wave Shaping which enables us to deliver an unmatched user experience to our end customers.”
New features for NXP’s NFC frontend solution include:
- Dynamic Power Control (DPC): DPC increases communication stability and reliability. It enables up to 30 percent increase of the effective transmitter current at the same maximum specification. It maximizes RF system performance, optimizes effective power output, and minimizes overall energy consumption by automatically compensating for detuning effects generated by nearby smartcards, NFC-enabled smart phones or metal objects. While enabling communication at long distance, the automated calibration avoids a possible damage in cards and phones caused by overpowering in zero distance.
- Simple Certification: The combined features of DPC, strong RF power and hardware-based EMD error handing eases certification. Being pre-certified for contactless EMVCo L1 and NFC Forum, PN5180 is ideal for designs that target payment applications. Additionally, the TFBGA package with added security features simplifies PCI terminal certification.
- Ease Design Process: The PN5180 is supported by advanced design-in software tools. The PC-based “NFC Cockpit” software environment is an intuitive graphical user interface that supports software-independent tuning of the antenna’s register settings, so hardware designers can optimize antenna parameters while software designers work on integration of the embedded system in parallel. PN5180 also comes with a completely overhauled NFC Reader Library which is easily portable to various controller cores. The library is pre-certified for EMVCo L1 and NFC Forum and complies with all applicable ISO/IEC standards.
Due to its advanced features, PN5180 was selected for the latest TWR-POS-K81, the latest Point of Sale reference design which is the first point solution from the recently merged companies NXP and Freescale. “PN5180 is a crucial element of NXP’s vision to bring NFC everywhere since it significantly eases the certification process – often the biggest challenge in NFC designs. Designers will spend less effort and time on antenna tuning, parameters settings and software adjustments,” said Rafael Sotomayor, senior vice president of secure mobile transactions business line at NXP. “During the next months, NXP will release new products in all NFC categories, NFC frontend, controller and connected tags solution, all with new features to improve connectivity and ease the design-in process.”
For more information about NXP’s NFC solutions visit, www.nxp.com.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 45,000 employees in more than 35 countries.
Forward-looking Statements
This document includes forward-looking statements which include statements regarding NXP’s business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by the United States federal securities laws, NXP does not have any intention or obligation to publicly update or revise any forward-looking statements after NXP distributes this document, whether to reflect any future events or circumstances or otherwise. For a discussion of potential risks and uncertainties, please refer to the risk factors listed in NXP’s SEC filings. Copies of NXP’s SEC filings are available from the SEC website, www.sec.gov.
For more information, please contact: AmericasTate TranTel: +1 408 802 0602Email: tate.tran@nxp.comGreater China/AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chan@nxp.comEuropeMartijn van der LindenPhone: +31 6 1091 4896Email: martijn.van.der.linden@nxp.com
NXP Semiconductors Netherlands B.V.