News Highlights:
For more than 50 years, 2.45 GHz magnetrons have been widely used in consumer and industrial applications ranging from microwave ovens to high power welding machines. Solid-state solutions appeared on the market several years ago, bringing advanced control, reliability, and ease of use. The capability to dynamically adjust the power, frequency, and phase helps optimize the energy transmitted to the material or food being heated. The long lifetime of transistors at full rated performance reduces the need for replacements. However, until the advent of GaN-on-SiC for RF Energy, solid-state devices lacked efficiency to meet the performance standards of the incumbent magnetrons.
The MRF24G300HS is a 330 W CW, 50 V GaN-on-SiC transistor, demonstrating 73 percent drain efficiency at 2.45 GHz, which is five points higher than the latest LDMOS technologies. The high power density of GaN enables the device to reach high output power in a small footprint. GaN technology has an inherently high output impedance that allows broadband matching compared to LDMOS. This reduces the design time and ensures consistency on the manufacturing line – no more hand tuning needed. The simplified gate biasing of the MRF24G300HS RF transistor removes another step of the otherwise complex power-up sequence typically seen on GaN devices.
“The smart control, low maintenance, and ease of use of solid-state open the door to new use cases, such as smart cooking and industry 4.0 heating machines,” said
Availability
NXP’s MRF24G300HS RF transistor is sampling now and production is planned for Q3 2019. The 2400-2500 MHz reference circuit is available now, under order number MRF24G300HS-2450MHZ. As part of the NXP Partner Program,
NXP Showcase at IMS 2019: The Microwave Hub
Stop by the NXP booth where the company will showcase “The Microwave Hub.” Visit the NXP booth# 548 to explore the possibilities of integrating more functions into a single device.
About
NXP and the NXP logo are trademarks of
For more information, please contact:
Americas | Europe | Greater China / Asia |
Tate Tran | Martijn van der Linden | Ming Yue |
Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +86 21 2205 2690 |
Email: tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: ming.yue@nxp.com |
Source: NXP USA, Inc.
Tags: Industrial