Select site:
English
Compliance testing at NXP HDMI ATC

There are three steps for a manufacturer to perform HDMI compliance testing at the NXP Semiconductors HDMI ATC.


1. Product submission

  • Only HDMI Adopters having a HDMI license in good standing can submit products for testing
  • An ATC Order Form must be completed and sent to the NXP Semiconductors ATC
  • A NDA between the manufacturer and the NXP Semiconductors ATC must be executed prior to testing
  • A HDMI Compliance Test Application specified in the HDMI Compliance Testing Policies and Procedures must be sent to the ATC
  • A Capabilities Declaration Form (CDF) specified in the HDMI Compliance Test Specification must be sent to the ATC

2. Testing

  • Submit product and any ancillary equipment (such as signal generators) required to operate the product. Product and ancillary equipment must include operating instructions
  • Equipment is shipped to the NXP Semiconductors HDMI ATC several days prior to testing. ATC personnel inspect the equipment. If any equipment or instructions are missing, ATC personnel will request replacements
  • The product is tested in accordance with the HDMI CTS 1.3b

3. Test results

  • HDMI compliance test results are reported to the manufacturer
  • In case the test results are positive, the ATC also sends a Confirmation Letter to the manufacturer
  • The product and ancillary equipment are returned to the manufacturer

Once the manufacturer receives the test results, they should submit the report and Confirmation letter to the HDMI Licensing LLC. The HDMI Licensing LLC will acknowledge receipt of the test results, indicating to the manufacturer that they may ship the product with the HDMI logo.


Test ordering numbers

NXHT111 - HDMI Source Device Testing (1 output)
NXHT113 - Additional Source Device Outputs
NXHT114 - HDMI Source Device Resubmission
NXHT131 - HDMI Sink Device Testing (1 input)
NXHT132 - Additional Sink Device Inputs
NXHT134 - HDMI Sink Device Resubmission
NXHT151 - HDMI Repeater Device Testing (1 input/1 output)
NXHT152 - Additional Repeater Device Inputs
NXHT153 - Additional Repeater Device Outputs
NXHT154 - HDMI Repeater Device Resubmission
NXHT171 - HDMI Cable Testing
NXHT174 - HDMI Cable Resubmission
NXHDCP - HDCP Compliance Testing


ATC ordering package

To arrange testing at NXP Semiconductors HDMI ATC, a manufacturer must have an ATC ordering package. This contains:


The Ordering Instructions document enclosed in the package gives detailed instructions for the ATC submission process. For more information or to receive an ATC Ordering Package, please send an Send a message e-mail or call +33 (0)2 31 45 64 21 and ask for the HDMI ATC Manager.